ExternalConnectionBuilder Class¶
-
class
NXOpen.Mechatronics.
ExternalConnectionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ExternalConnection
builderTo create a new instance of this class, use
NXOpen.Mechatronics.ExternalConnectionCollection.CreateExternalConnectionBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ConnectionList | Returns the connection element list. |
Name | Returns or sets the name. |
SelectPhysics | Returns the select physics. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddElement | Add one element. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
RemoveAllElements | Remove all elements. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ExternalConnectionBuilderConditionType Enumeration | the condition type. |
Property Detail¶
ConnectionList¶
-
ExternalConnectionBuilder.
ConnectionList
¶ Returns the connection element list.
-------------------------------------
Getter Method
Signature
ConnectionList
Returns: Return type: NXOpen.Mechatronics.ExternalConnectionElementBuilderList
New in version NX8.0.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Name¶
-
ExternalConnectionBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX8.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SelectPhysics¶
-
ExternalConnectionBuilder.
SelectPhysics
¶ Returns the select physics.
-------------------------------------
Getter Method
Signature
SelectPhysics
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
AddElement¶
-
ExternalConnectionBuilder.
AddElement
¶ Add one element.
Signature
AddElement(propTag, signalType, signalName, propertyType, streamIO, conditionType, conditionValue, multiplier, offsetValue, boolOperator)
Parameters: - propTag (int) –
- signalType (int) –
- signalName (str) –
- propertyType (int) –
- streamIO (int) –
- conditionType (int) –
- conditionValue (float) –
- multiplier (float) –
- offsetValue (float) –
- boolOperator (int) –
New in version NX8.0.0.
Deprecated since version NX8.0.1: Please use
NXOpen.Mechatronics.ExternalConnectionElementBuilder
instead.License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RemoveAllElements¶
-
ExternalConnectionBuilder.
RemoveAllElements
¶ Remove all elements.
Signature
RemoveAllElements()
New in version NX8.0.0.
Deprecated since version NX8.0.1: Please use
NXOpen.Mechatronics.ExternalConnectionElementBuilder
instead.License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
ExternalConnectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.