ComparisonResultAttribute Class¶
-
class
NXOpen.Mechatronics.
ComparisonResultAttribute
¶ Bases:
NXOpen.Mechatronics.ComparisonResultBase
Represents attribute of comparison result
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
EcadValue | Returns or sets the value of imported ECAD device object |
Ignored | Returns or sets the flag marked if the object will be ingored when applying it to logical model |
LogicalValue | Returns or sets the value of matched logical object |
Name | Returns the name of the attribute |
Property Detail¶
EcadValue¶
-
ComparisonResultAttribute.
EcadValue
¶ Returns or sets the value of imported ECAD device object
-------------------------------------
Getter Method
Signature
EcadValue
Returns: Value of imported ECAD device object Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EcadValue
Parameters: ecadValue (str) – Value of imported ECAD device object New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LogicalValue¶
-
ComparisonResultAttribute.
LogicalValue
¶ Returns or sets the value of matched logical object
-------------------------------------
Getter Method
Signature
LogicalValue
Returns: Value of matched logical object Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LogicalValue
Parameters: logicalValue (str) – Value of matched logical object New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Dispose¶
-
ComparisonResultAttribute.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX9.0.0.
License requirements: None.