ComparisonResultBase Class¶
-
class
NXOpen.Mechatronics.
ComparisonResultBase
¶ Bases:
NXOpen.TransientObject
Represents base object of comparison result
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Ignored | Returns or sets the flag marked if the object will be ingored when applying it to logical model |
Property Detail¶
Ignored¶
-
ComparisonResultBase.
Ignored
¶ Returns or sets the flag marked if the object will be ingored when applying it to logical model
-------------------------------------
Getter Method
Signature
Ignored
Returns: Mark if the object will be ingored when applying it to logical model Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Ignored
Parameters: isIgnored (bool) – Mark if the object will be ingored when applying it to logical model New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Dispose¶
-
ComparisonResultBase.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX9.0.0.
License requirements: None.