BreakingConstraintCollection Class

class NXOpen.Mechatronics.BreakingConstraintCollection

Bases: object

Represents a collection of Breaking Constraint.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX7.5.1.

Method Detail

CreateBreakingConstraintBuilder

BreakingConstraintCollection.CreateBreakingConstraintBuilder

Creates a NXOpen.Mechatronics.BreakingConstraintBuilder.

Signature CreateBreakingConstraintBuilder(hinge)

Parameters:hinge (NXOpen.Mechatronics.BreakingConstraint) – NXOpen.Mechatronics.BreakingConstraint to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.BreakingConstraintBuilder

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

BreakingConstraintCollection.FindObject

Finds the NXOpen.Mechatronics.BreakingConstraint with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.BreakingConstraint.
Returns:NXOpen.Mechatronics.BreakingConstraint with this name.
Return type:NXOpen.Mechatronics.BreakingConstraint

New in version NX7.5.1.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)