BreakingConstraintBuilder Class¶
-
class
NXOpen.Mechatronics.
BreakingConstraintBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsConstraintBuilder
Represents a
NXOpen.Mechatronics.BreakingConstraint
builder.To create a new instance of this class, use
NXOpen.Mechatronics.BreakingConstraintCollection.CreateBreakingConstraintBuilder()
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
BreakingMode | Returns or sets the breaking mode. |
Direction | Returns or sets the direction. |
FixedDirection | Returns or sets the direction is fixed or not. |
Joint | Returns the joint object. |
MaximumMagnitude | Returns the maximum allowable magnitude, the joint will be broken if it exceeds this value. |
Name | Returns or sets the name. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetJoint | Sets the joint. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BreakingConstraintBuilderBreakingModeType Enumeration | Represents the breaking mode. |
Property Detail¶
BreakingMode¶
-
BreakingConstraintBuilder.
BreakingMode
¶ Returns or sets the breaking mode.
-------------------------------------
Getter Method
Signature
BreakingMode
Returns: Return type: NXOpen.Mechatronics.BreakingConstraintBuilderBreakingModeType
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
BreakingMode
Parameters: breakingMode ( NXOpen.Mechatronics.BreakingConstraintBuilderBreakingModeType
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Direction¶
-
BreakingConstraintBuilder.
Direction
¶ Returns or sets the direction.
-------------------------------------
Getter Method
Signature
Direction
Returns: Return type: NXOpen.Direction
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Direction
Parameters: direction ( NXOpen.Direction
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FixedDirection¶
-
BreakingConstraintBuilder.
FixedDirection
¶ Returns or sets the direction is fixed or not.
-------------------------------------
Getter Method
Signature
FixedDirection
Returns: Return type: bool New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
FixedDirection
Parameters: fixedDirection (bool) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Joint¶
-
BreakingConstraintBuilder.
Joint
¶ Returns the joint object.
It can be any type of joints.
-------------------------------------
Getter Method
Signature
Joint
Returns: Return type: NXOpen.Mechatronics.SelectPhysicsJoint
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MaximumMagnitude¶
-
BreakingConstraintBuilder.
MaximumMagnitude
¶ Returns the maximum allowable magnitude, the joint will be broken if it exceeds this value.
-------------------------------------
Getter Method
Signature
MaximumMagnitude
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
SetJoint¶
-
BreakingConstraintBuilder.
SetJoint
¶ Sets the joint.
Signature
SetJoint(joint)
Parameters: joint ( NXOpen.Mechatronics.PhysicsJoint
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
BreakingConstraintBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.