AnimationConversionBuilder Class¶
-
class
NXOpen.Mechatronics.
AnimationConversionBuilder
¶ Bases:
NXOpen.Builder
Represents a
Mechatronics.AnimationConversionBuilder
builderTo create a new instance of this class, use
NXOpen.Mechatronics.PhysicsManager.CreateAnimationConversionBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EnableObjectsConversion | Enables the conversion of objects. If it is impossible, the objects will keep unable status. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetTentativePhysics | Returns the tentatively converting physics objects. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Associative¶
-
AnimationConversionBuilder.
Associative
¶ Returns or sets the associative.
-------------------------------------
Getter Method
Signature
Associative
Returns: Return type: bool New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Associative
Parameters: associative (bool) – New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
EnableObjectsConversion¶
-
AnimationConversionBuilder.
EnableObjectsConversion
¶ Enables the conversion of objects. If it is impossible, the objects will keep unable status.
Signature
EnableObjectsConversion(physics, enable)
Parameters: - physics (list of
NXOpen.NXObject
) – - enable (bool) –
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
- physics (list of
GetTentativePhysics¶
-
AnimationConversionBuilder.
GetTentativePhysics
¶ Returns the tentatively converting physics objects.
Signature
GetTentativePhysics()
Returns: Return type: list of NXOpen.NXObject
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
AnimationConversionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.