SplitBuilder Class¶
-
class
NXOpen.MechanicalRouting.
SplitBuilder
¶ Bases:
NXOpen.Builder
the Builder to Assign Discontinuity for the stocks
To create a new instance of this class, use
NXOpen.MechanicalRouting.BuilderFactory.CreateSplitBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ControlPointCollector | Returns the Rcp type of the selected object |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCreatedComponents | Components created during Split operation. |
GetLogicalObjects | Returns the :py:class:`PDM.LogicalObject`s that represent content that will be created by this builder. |
GetObject | Returns the object currently being edited by this builder. |
PreCommit | Performs the operations needed prior to a commit. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ControlPointCollector¶
-
SplitBuilder.
ControlPointCollector
¶ Returns the Rcp type of the selected object
-------------------------------------
Getter Method
Signature
ControlPointCollector
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
GetCreatedComponents¶
-
SplitBuilder.
GetCreatedComponents
¶ Components created during Split operation.
Signature
GetCreatedComponents()
Returns: Components created during Split operation. Return type: list of NXOpen.Assemblies.Component
New in version NX11.0.1.
License requirements: routing_base (“Routing Basic”)
GetLogicalObjects¶
-
SplitBuilder.
GetLogicalObjects
¶ Returns the :py:class:`PDM.LogicalObject`s that represent content that will be created by this builder.
Signature
GetLogicalObjects()
Returns: Return type: list of NXOpen.PDM.LogicalObject
New in version NX11.0.1.
License requirements: routing_base (“Routing Basic”)
PreCommit¶
-
SplitBuilder.
PreCommit
¶ Performs the operations needed prior to a commit.
This method has to be called before invoking commit.
Signature
PreCommit()
New in version NX11.0.1.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
SplitBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.