InsulationService Class¶
-
class
NXOpen.MechanicalRouting.
InsulationService
¶ Bases:
object
Represents a
NXOpen.MechanicalRouting.InsulationService
object.Uses the
MechanicalRouting.RoutingManager.InsulationService()
to obtain an instance of this class.To obtain an instance of this class, refer to
NXOpen.MechanicalRouting.RoutingManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
GetAllInsulatedObjectsInContainer | Get all insulation occurences in current container |
Method Detail¶
GetAllInsulatedObjectsInContainer¶
-
InsulationService.
GetAllInsulatedObjectsInContainer
¶ Get all insulation occurences in current container
Signature
GetAllInsulatedObjectsInContainer(container)
Parameters: container ( NXOpen.Assemblies.Component
) –Returns: Return type: list of NXOpen.NXObject
New in version NX12.0.0.
License requirements: routing_pipetube (“Routing Piping and Tubing”)