MeasureBuilder Class¶
-
class
NXOpen.
MeasureBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.MeasureBuilder
This is an abstract class, and cannot be instantiated.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AnnotationMode | Returns or sets the annotation mode |
InfoWindow | Returns or sets the info window |
RequirementMode | Returns or sets the requirement mode |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MeasureBuilderAnnotationType Enumeration | Represents the annotation type. |
MeasureBuilderRequirementType Enumeration | Represents the requirement type. |
Property Detail¶
AnnotationMode¶
-
MeasureBuilder.
AnnotationMode
¶ Returns or sets the annotation mode
-------------------------------------
Getter Method
Signature
AnnotationMode
Returns: Return type: NXOpen.MeasureBuilderAnnotationType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnnotationMode
Parameters: atype ( NXOpen.MeasureBuilderAnnotationType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
InfoWindow¶
-
MeasureBuilder.
InfoWindow
¶ Returns or sets the info window
-------------------------------------
Getter Method
Signature
InfoWindow
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InfoWindow
Parameters: infoWindow (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RequirementMode¶
-
MeasureBuilder.
RequirementMode
¶ Returns or sets the requirement mode
-------------------------------------
Getter Method
Signature
RequirementMode
Returns: Return type: NXOpen.MeasureBuilderRequirementType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RequirementMode
Parameters: rtype ( NXOpen.MeasureBuilderRequirementType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
MeasureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.