MeasureBuilderRequirementType Enumeration

NXOpen.MeasureBuilder.RequirementType is an alias for NXOpen.MeasureBuilderRequirementType

class NXOpen.MeasureBuilderRequirementType

Bases: object

Represents the requirement type.

Enum Members

Enum Member Enum Member Description
NotSet
New
Existing
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.