MeasureAngleBuilder Class¶
-
class
NXOpen.
MeasureAngleBuilder
¶ Bases:
NXOpen.MeasureBuilder
Represents a
NXOpen.MeasureAngleBuilder
To create a new instance of this class, use
NXOpen.MeasureManager.CreateMeasureAngleBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AnnotationMode | Returns or sets the annotation mode |
BaseEnd | Returns or sets the end point |
BasePoint | Returns or sets the base point |
Feature1 | Returns the feature1 |
Feature2 | Returns the feature2 |
InfoWindow | Returns or sets the info window |
IsExact | Returns or sets the exact flag |
Object1 | Returns the object1 |
Object2 | Returns the object2 |
Objtype1 | Returns or sets the otype1 |
Objtype2 | Returns or sets the otype2 |
Orientation | Returns or sets the orientation |
ProtractorEnd | Returns or sets the protractor end point |
Ptype | Returns or sets the ptype |
RequirementMode | Returns or sets the requirement mode |
Tag | Returns the Tag for this object. |
Vector1 | Returns or sets the vector1 |
Vector2 | Returns or sets the vector2 |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MeasureAngleBuilderAngleType Enumeration | Represents the angle type. |
MeasureAngleBuilderObjectType Enumeration | Represents the object type. |
MeasureAngleBuilderOrientationType Enumeration | Represents the orientation type |
MeasureAngleBuilderProjectionType Enumeration | Represents the projection type. |
Property Detail¶
BaseEnd¶
-
MeasureAngleBuilder.
BaseEnd
¶ Returns or sets the end point
-------------------------------------
Getter Method
Signature
BaseEnd
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
BaseEnd
Parameters: baseEnd ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
BasePoint¶
-
MeasureAngleBuilder.
BasePoint
¶ Returns or sets the base point
-------------------------------------
Getter Method
Signature
BasePoint
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
BasePoint
Parameters: basePoint ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Feature1¶
-
MeasureAngleBuilder.
Feature1
¶ Returns the feature1
-------------------------------------
Getter Method
Signature
Feature1
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX5.0.0.
License requirements: None.
Feature2¶
-
MeasureAngleBuilder.
Feature2
¶ Returns the feature2
-------------------------------------
Getter Method
Signature
Feature2
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX5.0.0.
License requirements: None.
IsExact¶
-
MeasureAngleBuilder.
IsExact
¶ Returns or sets the exact flag
-------------------------------------
Getter Method
Signature
IsExact
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsExact
Parameters: isExact (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Object1¶
-
MeasureAngleBuilder.
Object1
¶ Returns the object1
-------------------------------------
Getter Method
Signature
Object1
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX5.0.0.
License requirements: None.
Object2¶
-
MeasureAngleBuilder.
Object2
¶ Returns the object2
-------------------------------------
Getter Method
Signature
Object2
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX5.0.0.
License requirements: None.
Objtype1¶
-
MeasureAngleBuilder.
Objtype1
¶ Returns or sets the otype1
-------------------------------------
Getter Method
Signature
Objtype1
Returns: Return type: NXOpen.MeasureAngleBuilderObjectType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Objtype1
Parameters: objtype ( NXOpen.MeasureAngleBuilderObjectType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Objtype2¶
-
MeasureAngleBuilder.
Objtype2
¶ Returns or sets the otype2
-------------------------------------
Getter Method
Signature
Objtype2
Returns: Return type: NXOpen.MeasureAngleBuilderObjectType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Objtype2
Parameters: objtype ( NXOpen.MeasureAngleBuilderObjectType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Orientation¶
-
MeasureAngleBuilder.
Orientation
¶ Returns or sets the orientation
-------------------------------------
Getter Method
Signature
Orientation
Returns: Return type: NXOpen.MeasureAngleBuilderOrientationType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Orientation
Parameters: mtype ( NXOpen.MeasureAngleBuilderOrientationType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ProtractorEnd¶
-
MeasureAngleBuilder.
ProtractorEnd
¶ Returns or sets the protractor end point
-------------------------------------
Getter Method
Signature
ProtractorEnd
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
ProtractorEnd
Parameters: protractorEnd ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Ptype¶
-
MeasureAngleBuilder.
Ptype
¶ Returns or sets the ptype
-------------------------------------
Getter Method
Signature
Ptype
Returns: Return type: NXOpen.MeasureAngleBuilderProjectionType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Ptype
Parameters: mtype ( NXOpen.MeasureAngleBuilderProjectionType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Vector1¶
-
MeasureAngleBuilder.
Vector1
¶ Returns or sets the vector1
-------------------------------------
Getter Method
Signature
Vector1
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector1
Parameters: vector1 ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Vector2¶
-
MeasureAngleBuilder.
Vector2
¶ Returns or sets the vector2
-------------------------------------
Getter Method
Signature
Vector2
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector2
Parameters: vector2 ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
MeasureAngleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.