RailOpeningFeatureBuilder Class¶
-
class
NXOpen.LineDesigner.
RailOpeningFeatureBuilder
¶ Bases:
NXOpen.Builder
Represents a
LineDesigner.RailOpeningFeature
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateRailOpeningFeatureBuilder()
Default values.
Property Value LinearDimElevation.Value 650 (millimeters part), 25.6 (inches part) LinearDimGateThickness.Value 37.5 (millimeters part), 1.5 (inches part) LinearDimOpeningWidth.Value 350 (millimeters part), 14 (inches part) OpeningAddGate 0 OpeningStyleEnum Left New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
LinearDimElevation | Returns the rail opening elevation |
LinearDimGateThickness | Returns the gate thickness |
LinearDimOpeningWidth | Returns the rail opening width |
OpeningAddGate | Returns or sets the opening add gate is return |
OpeningStyleEnum | Returns or sets the rail opening style enum |
ReverseDirection | Returns or sets the reverse direction of rail opening |
SelectPoint | Returns or sets the selected point of rail opening feature |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDirVector | Direction of rail opening |
GetObject | Returns the object currently being edited by this builder. |
SetDirVector | |
SetRailingFeature | |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RailOpeningFeatureBuilderGateOpeningStyle Enumeration | This enum is providing possible gate opening styles |
Property Detail¶
LinearDimElevation¶
-
RailOpeningFeatureBuilder.
LinearDimElevation
¶ Returns the rail opening elevation
-------------------------------------
Getter Method
Signature
LinearDimElevation
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimGateThickness¶
-
RailOpeningFeatureBuilder.
LinearDimGateThickness
¶ Returns the gate thickness
-------------------------------------
Getter Method
Signature
LinearDimGateThickness
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimOpeningWidth¶
-
RailOpeningFeatureBuilder.
LinearDimOpeningWidth
¶ Returns the rail opening width
-------------------------------------
Getter Method
Signature
LinearDimOpeningWidth
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
OpeningAddGate¶
-
RailOpeningFeatureBuilder.
OpeningAddGate
¶ Returns or sets the opening add gate is return
-------------------------------------
Getter Method
Signature
OpeningAddGate
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
OpeningAddGate
Parameters: openingAddGate (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
OpeningStyleEnum¶
-
RailOpeningFeatureBuilder.
OpeningStyleEnum
¶ Returns or sets the rail opening style enum
-------------------------------------
Getter Method
Signature
OpeningStyleEnum
Returns: Return type: NXOpen.LineDesigner.RailOpeningFeatureBuilderGateOpeningStyle
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
OpeningStyleEnum
Parameters: openingStyleEnum ( NXOpen.LineDesigner.RailOpeningFeatureBuilderGateOpeningStyle
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ReverseDirection¶
-
RailOpeningFeatureBuilder.
ReverseDirection
¶ Returns or sets the reverse direction of rail opening
-------------------------------------
Getter Method
Signature
ReverseDirection
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ReverseDirection
Parameters: reverseDirection (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SelectPoint¶
-
RailOpeningFeatureBuilder.
SelectPoint
¶ Returns or sets the selected point of rail opening feature
-------------------------------------
Getter Method
Signature
SelectPoint
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SelectPoint
Parameters: selectPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
GetDirVector¶
-
RailOpeningFeatureBuilder.
GetDirVector
¶ Direction of rail opening
Signature
GetDirVector()
Returns: Return type: NXOpen.Direction
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetDirVector¶
-
RailOpeningFeatureBuilder.
SetDirVector
¶ Signature
SetDirVector(dirVector)
Parameters: dirVector ( NXOpen.Direction
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetRailingFeature¶
-
RailOpeningFeatureBuilder.
SetRailingFeature
¶ Signature
SetRailingFeature(railingFrec)
Parameters: railingFrec ( NXOpen.Features.Feature
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
RailOpeningFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.