HoleFeatureBuilder Class¶
-
class
NXOpen.LineDesigner.
HoleFeatureBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
LineDesigner.HoleFeature
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateHoleFeatureBuilder()
Default values.
Property Value AddCover 0 CoverThickness.Value 127 (millimeters part), 5 (inches part) LoadRequirements 0 TextSize 60 UseCoverOffset 0 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AddCover | Returns or sets the presence of cover over hole is checked |
CoverThickness | Returns the cover thickness |
LoadRequirements | Returns or sets the load requirements |
MakeSketchInternal | Returns or sets |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SelectOutline | Returns the selected outline for creation of hole |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TextLocation | Returns or sets the text location of hole |
TextSize | Returns or sets the text size |
UseCoverOffset | Returns or sets the cover offset is return, if cover is present over hole |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetEnterTextString | Get text string |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetEnterTextString | Set text string |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AddCover¶
-
HoleFeatureBuilder.
AddCover
¶ Returns or sets the presence of cover over hole is checked
-------------------------------------
Getter Method
Signature
AddCover
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
AddCover
Parameters: addCover (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
CoverThickness¶
-
HoleFeatureBuilder.
CoverThickness
¶ Returns the cover thickness
-------------------------------------
Getter Method
Signature
CoverThickness
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LoadRequirements¶
-
HoleFeatureBuilder.
LoadRequirements
¶ Returns or sets the load requirements
-------------------------------------
Getter Method
Signature
LoadRequirements
Returns: Return type: float New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
LoadRequirements
Parameters: loadRequirements (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
MakeSketchInternal¶
-
HoleFeatureBuilder.
MakeSketchInternal
¶ Returns or sets
-------------------------------------
Getter Method
Signature
MakeSketchInternal
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
MakeSketchInternal
Parameters: makeSketchInternal (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SelectOutline¶
-
HoleFeatureBuilder.
SelectOutline
¶ Returns the selected outline for creation of hole
-------------------------------------
Getter Method
Signature
SelectOutline
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
TextLocation¶
-
HoleFeatureBuilder.
TextLocation
¶ Returns or sets the text location of hole
-------------------------------------
Getter Method
Signature
TextLocation
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
TextLocation
Parameters: textLocation ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
TextSize¶
-
HoleFeatureBuilder.
TextSize
¶ Returns or sets the text size
-------------------------------------
Getter Method
Signature
TextSize
Returns: Return type: float New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
TextSize
Parameters: textSize (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UseCoverOffset¶
-
HoleFeatureBuilder.
UseCoverOffset
¶ Returns or sets the cover offset is return, if cover is present over hole
-------------------------------------
Getter Method
Signature
UseCoverOffset
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
UseCoverOffset
Parameters: useCoverOffset (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
GetEnterTextString¶
-
HoleFeatureBuilder.
GetEnterTextString
¶ Get text string
Signature
GetEnterTextString()
Returns: Return type: list of str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetEnterTextString¶
-
HoleFeatureBuilder.
SetEnterTextString
¶ Set text string
Signature
SetEnterTextString(enterTextString)
Parameters: enterTextString (list of str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
HoleFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.