ConveyorStationFeatureBuilder Class¶
-
class
NXOpen.LineDesigner.
ConveyorStationFeatureBuilder
¶ Bases:
NXOpen.Builder
Represents a
LineDesigner.ConveyorStationFeature
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateConveyorStationFeatureBuilder()
Default values.
Property Value Capacity 0 ProcessTime 0 StationType Load New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Capacity | Returns or sets the conveyor station capacity |
ProcessTime | Returns or sets the Process time |
StationLocation | Returns or sets the conveyor station location |
StationName | Returns or sets the station name |
StationType | Returns or sets the conveyor station type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDescription | Description of conveyor station is return |
GetObject | Returns the object currently being edited by this builder. |
SetDescription | Description for conveyor station is set |
SetSECNode | |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConveyorStationFeatureBuilderType Enumeration | This enum is providing possible types of station feature |
Property Detail¶
Capacity¶
-
ConveyorStationFeatureBuilder.
Capacity
¶ Returns or sets the conveyor station capacity
-------------------------------------
Getter Method
Signature
Capacity
Returns: Return type: float New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
Capacity
Parameters: capacity (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ProcessTime¶
-
ConveyorStationFeatureBuilder.
ProcessTime
¶ Returns or sets the Process time
-------------------------------------
Getter Method
Signature
ProcessTime
Returns: Return type: float New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ProcessTime
Parameters: processTime (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StationLocation¶
-
ConveyorStationFeatureBuilder.
StationLocation
¶ Returns or sets the conveyor station location
-------------------------------------
Getter Method
Signature
StationLocation
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StationLocation
Parameters: stationLocation ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StationName¶
-
ConveyorStationFeatureBuilder.
StationName
¶ Returns or sets the station name
-------------------------------------
Getter Method
Signature
StationName
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StationName
Parameters: stationName (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StationType¶
-
ConveyorStationFeatureBuilder.
StationType
¶ Returns or sets the conveyor station type
-------------------------------------
Getter Method
Signature
StationType
Returns: Return type: NXOpen.LineDesigner.ConveyorStationFeatureBuilderType
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StationType
Parameters: stationType ( NXOpen.LineDesigner.ConveyorStationFeatureBuilderType
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
GetDescription¶
-
ConveyorStationFeatureBuilder.
GetDescription
¶ Description of conveyor station is return
Signature
GetDescription()
Returns: Return type: list of str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetDescription¶
-
ConveyorStationFeatureBuilder.
SetDescription
¶ Description for conveyor station is set
Signature
SetDescription(description)
Parameters: description (list of str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetSECNode¶
-
ConveyorStationFeatureBuilder.
SetSECNode
¶ Signature
SetSECNode(secNode)
Parameters: secNode ( NXOpen.LineDesigner.DBConveyorNode
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
ConveyorStationFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.