ConveyorStationFeatureBuilderType Enumeration¶
NXOpen.LineDesigner.ConveyorStationFeatureBuilder.Type is an alias for NXOpen.LineDesigner.ConveyorStationFeatureBuilderType
-
class
NXOpen.LineDesigner.
ConveyorStationFeatureBuilderType
¶ Bases:
object
This enum is providing possible types of station feature
Enum Members
Enum Member Enum Member Description Load Unload ProcessRun ProcessStop Idle Decision Marriage Disassembly Assembly Stop LimitSwitch ProximitySwitch Reader Pusher -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-