ColumnFeatureBuilder Class¶
-
class
NXOpen.LineDesigner.
ColumnFeatureBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
LineDesigner.ColumnFeature
Features.FeatureBuilder
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateColumnFeatureBuilder()
Default values.
Property Value BaseDepth.Value 800 (millimeters part), 32 (inches part) BaseDiameter.Value 800 (millimeters part), 32 (inches part) BaseHeight.Value 900 (millimeters part), 35 (inches part) BaseLowerDiameter.Value 900 (millimeters part), 35 (inches part) BaseStyleEnum None BaseUpperDiameter.Value 800 (millimeters part), 32 (inches part) BaseWidth.Value 800 (millimeters part), 32 (inches part) ColumnDepth.Value 600 (millimeters part), 25 (inches part) ColumnDiameter.Value 300 (millimeters part), 12 (inches part) ColumnHeight.Value 3000 (millimeters part), 120 (inches part) ColumnStyleEnum IBeam ColumnThickness.Value 30 (millimeters part), 2 (inches part) ColumnWidth.Value 600 (millimeters part), 25 (inches part) New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
BaseDepth | Returns the base depth of column feature |
BaseDiameter | Returns the base diameter of column feature |
BaseHeight | Returns the base height of column feature |
BaseLowerDiameter | Returns the base lower diameter of column feature |
BaseStyleEnum | Returns or sets the base cross section type of column feature |
BaseUpperDiameter | Returns the base upper diameter of column feature |
BaseUserDefineSuperSection | Returns the user define cross section for base of column feature |
BaseWidth | Returns the base width of column feature |
ColumnDepth | Returns the column depth of column feature |
ColumnDiameter | Returns the column diameter of column feature |
ColumnHeight | Returns the column height of column feature |
ColumnOriginPoint | Returns or sets the column origin point is returns where colums is created |
ColumnStyleEnum | Returns or sets the column style of column feature |
ColumnThickness | Returns the column thickness of column feature |
ColumnUserDefineSuperSection | Returns the user defined cross section of column feature |
ColumnWidth | Returns the column width of column feature |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ColumnFeatureBuilderColumnBaseType Enumeration | This enum is providing possible column base types |
ColumnFeatureBuilderColumnType Enumeration | This enum is providing possible column types |
Property Detail¶
BaseDepth¶
-
ColumnFeatureBuilder.
BaseDepth
¶ Returns the base depth of column feature
-------------------------------------
Getter Method
Signature
BaseDepth
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseDiameter¶
-
ColumnFeatureBuilder.
BaseDiameter
¶ Returns the base diameter of column feature
-------------------------------------
Getter Method
Signature
BaseDiameter
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseHeight¶
-
ColumnFeatureBuilder.
BaseHeight
¶ Returns the base height of column feature
-------------------------------------
Getter Method
Signature
BaseHeight
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseLowerDiameter¶
-
ColumnFeatureBuilder.
BaseLowerDiameter
¶ Returns the base lower diameter of column feature
-------------------------------------
Getter Method
Signature
BaseLowerDiameter
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseStyleEnum¶
-
ColumnFeatureBuilder.
BaseStyleEnum
¶ Returns or sets the base cross section type of column feature
-------------------------------------
Getter Method
Signature
BaseStyleEnum
Returns: Return type: NXOpen.LineDesigner.ColumnFeatureBuilderColumnBaseType
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
BaseStyleEnum
Parameters: baseStyleEnum ( NXOpen.LineDesigner.ColumnFeatureBuilderColumnBaseType
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseUpperDiameter¶
-
ColumnFeatureBuilder.
BaseUpperDiameter
¶ Returns the base upper diameter of column feature
-------------------------------------
Getter Method
Signature
BaseUpperDiameter
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseUserDefineSuperSection¶
-
ColumnFeatureBuilder.
BaseUserDefineSuperSection
¶ Returns the user define cross section for base of column feature
-------------------------------------
Getter Method
Signature
BaseUserDefineSuperSection
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseWidth¶
-
ColumnFeatureBuilder.
BaseWidth
¶ Returns the base width of column feature
-------------------------------------
Getter Method
Signature
BaseWidth
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnDepth¶
-
ColumnFeatureBuilder.
ColumnDepth
¶ Returns the column depth of column feature
-------------------------------------
Getter Method
Signature
ColumnDepth
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnDiameter¶
-
ColumnFeatureBuilder.
ColumnDiameter
¶ Returns the column diameter of column feature
-------------------------------------
Getter Method
Signature
ColumnDiameter
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnHeight¶
-
ColumnFeatureBuilder.
ColumnHeight
¶ Returns the column height of column feature
-------------------------------------
Getter Method
Signature
ColumnHeight
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnOriginPoint¶
-
ColumnFeatureBuilder.
ColumnOriginPoint
¶ Returns or sets the column origin point is returns where colums is created
-------------------------------------
Getter Method
Signature
ColumnOriginPoint
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ColumnOriginPoint
Parameters: columnOriginPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnStyleEnum¶
-
ColumnFeatureBuilder.
ColumnStyleEnum
¶ Returns or sets the column style of column feature
-------------------------------------
Getter Method
Signature
ColumnStyleEnum
Returns: Return type: NXOpen.LineDesigner.ColumnFeatureBuilderColumnType
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ColumnStyleEnum
Parameters: columnStyleEnum ( NXOpen.LineDesigner.ColumnFeatureBuilderColumnType
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnThickness¶
-
ColumnFeatureBuilder.
ColumnThickness
¶ Returns the column thickness of column feature
-------------------------------------
Getter Method
Signature
ColumnThickness
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnUserDefineSuperSection¶
-
ColumnFeatureBuilder.
ColumnUserDefineSuperSection
¶ Returns the user defined cross section of column feature
-------------------------------------
Getter Method
Signature
ColumnUserDefineSuperSection
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnWidth¶
-
ColumnFeatureBuilder.
ColumnWidth
¶ Returns the column width of column feature
-------------------------------------
Getter Method
Signature
ColumnWidth
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
ColumnFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.