LayoutCollection Class¶
-
class
NXOpen.
LayoutCollection
¶ Bases:
object
Represents a collection of layouts.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
ChangeLayout | Sets the given layout as current layout |
ChangeLayoutWithOptions | Sets the given layout as current layout and optionally removes the old and/or new layout caches |
Create | Creates a layout using an NXOpen.LayoutDefinition . |
CreateSplitScreenLayoutAndNamedViews | This method creates a layout with two modeling views. |
DestroySplitScreenLayoutAndNamedViews | This method destroys the split screen layout along with the views * that are there in it |
FindObject | Finds the NXOpen.Layout with the given identifier as recorded in a journal. |
NewLayoutDefinition | Constructs a NXOpen.LayoutDefinition object to be used to create a layout. |
RenameViewsInSplitScreenLayout | Using given names renames the views in split screen layout. |
Property Detail¶
Current¶
-
LayoutCollection.
Current
¶ Returns the current layout of the part.
When in the drafting application and a drawing sheet is not displayed, this will return a layout that has limited operations that can be performed on it.
-------------------------------------
Getter Method
Signature
Current
Returns: Return type: NXOpen.Layout
New in version NX3.0.0.
License requirements: None.
Method Detail¶
ChangeLayout¶
-
LayoutCollection.
ChangeLayout
¶ Sets the given layout as current layout
Signature
ChangeLayout(layout)
Parameters: layout ( NXOpen.Layout
) – LayoutNew in version NX6.0.0.
License requirements: None.
ChangeLayoutWithOptions¶
-
LayoutCollection.
ChangeLayoutWithOptions
¶ Sets the given layout as current layout and optionally removes the old and/or new layout caches
Signature
ChangeLayoutWithOptions(layout, removeOldLayoutCache, ignoreNewLayoutCache)
Parameters: - layout (
NXOpen.Layout
) – Layout - removeOldLayoutCache (bool) – Flag to indicate if the current layout’s cache should be removed
- ignoreNewLayoutCache (bool) – Flag to indicate if the new layout’s cache should be used or removed
New in version NX11.0.0.
License requirements: None.
- layout (
Create¶
-
LayoutCollection.
Create
¶ Creates a layout using an
NXOpen.LayoutDefinition
.Signature
Create(name, layoutArrangement, fitAllViews)
Parameters: - name (str) – Name of layout
- layoutArrangement (
NXOpen.LayoutDefinition
) – Arrangement and view location information - fitAllViews (bool) – Flag that indicates for the system to perform a fit before displaying the view. Otherwise the system displays the view at the scale at which it was last saved.
Returns: Return type: New in version NX3.0.0.
License requirements: None.
CreateSplitScreenLayoutAndNamedViews¶
-
LayoutCollection.
CreateSplitScreenLayoutAndNamedViews
¶ This method creates a layout with two modeling views.
The views ** are created with names given. Layout and view tags are returned
Signature
CreateSplitScreenLayoutAndNamedViews(leftViewName, rightViewname)
Parameters: - leftViewName (str) – name for the left view
- rightViewname (str) – name for the right view
Returns: a tuple
Return type: A tuple consisting of (layout, leftView, rightView). layout is a
NXOpen.Layout
. Layout leftView is aNXOpen.View
. View rightView is aNXOpen.View
. ViewNew in version NX6.0.0.
License requirements: None.
DestroySplitScreenLayoutAndNamedViews¶
-
LayoutCollection.
DestroySplitScreenLayoutAndNamedViews
¶ This method destroys the split screen layout along with the views * that are there in it
Signature
DestroySplitScreenLayoutAndNamedViews(layout)
Parameters: layout ( NXOpen.Layout
) – LayoutNew in version NX6.0.0.
License requirements: None.
FindObject¶
-
LayoutCollection.
FindObject
¶ Finds the
NXOpen.Layout
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Layout found Return type: NXOpen.Layout
New in version NX3.0.0.
License requirements: None.
NewLayoutDefinition¶
-
LayoutCollection.
NewLayoutDefinition
¶ Constructs a
NXOpen.LayoutDefinition
object to be used to create a layout.If a layout is not created using the created definition object, the client is responsible for deleting it.
Signature
NewLayoutDefinition(arrangement)
Parameters: arrangement ( NXOpen.LayoutDefinitionArrangementType
) – Arrangement typeReturns: Layout arrangement used to create a layout :rtype:
NXOpen.LayoutDefinition
New in version NX3.0.0.
License requirements: None.
RenameViewsInSplitScreenLayout¶
-
LayoutCollection.
RenameViewsInSplitScreenLayout
¶ Using given names renames the views in split screen layout.
Signature
RenameViewsInSplitScreenLayout(layout, leftViewName, rightViewName)
Parameters: - layout (
NXOpen.Layout
) – Layout - leftViewName (str) – name for the left view
- rightViewName (str) – name for the right view
New in version NX6.0.0.
License requirements: None.
- layout (