LayoutDefinitionArrangementType Enumeration¶
NXOpen.LayoutDefinition.ArrangementType is an alias for NXOpen.LayoutDefinitionArrangementType
-
class
NXOpen.
LayoutDefinitionArrangementType
¶ Bases:
object
Indicates the arrangement type of a layout.
New in version NX3.0.0.
Enum Members
Enum Member Enum Member Description L1 One row by one column L2 One row by two columns L3 Two rows by one column L4 Two rows by two columns L6 Two rows by three columns L9 Three rows by three columns NonStandard A non standard layout. A layout definition cannot be made with this option. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-