SupportPlaneData Class¶
-
class
NXOpen.GeometricUtilities.
SupportPlaneData
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.SupportPlaneData
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ExistingPlane | Returns or sets the existing face or plane |
SupportPlane | Returns or sets the support plane |
SupportPlaneLockStatus | Returns or sets the support plane lock status |
Tag | Returns the Tag for this object. |
WorkView | Returns or sets the work view required when lock plane status is NXOpen.GeometricUtilities.SupportPlaneDataLockPlaneStatus.AfterFirstConstraint |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SupportPlaneDataLockPlaneStatus Enumeration | Represents support plane lock status for associative basic curves |
Property Detail¶
ExistingPlane¶
-
SupportPlaneData.
ExistingPlane
¶ Returns or sets the existing face or plane
-------------------------------------
Getter Method
Signature
ExistingPlane
Returns: Return type: NXOpen.DisplayableObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExistingPlane
Parameters: existingPlane ( NXOpen.DisplayableObject
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
SupportPlane¶
-
SupportPlaneData.
SupportPlane
¶ Returns or sets the support plane
-------------------------------------
Getter Method
Signature
SupportPlane
Returns: Return type: NXOpen.Plane
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SupportPlane
Parameters: supportPlane ( NXOpen.Plane
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
SupportPlaneLockStatus¶
-
SupportPlaneData.
SupportPlaneLockStatus
¶ Returns or sets the support plane lock status
-------------------------------------
Getter Method
Signature
SupportPlaneLockStatus
Returns: Return type: NXOpen.GeometricUtilities.SupportPlaneDataLockPlaneStatus
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SupportPlaneLockStatus
Parameters: lockPlaneStatus ( NXOpen.GeometricUtilities.SupportPlaneDataLockPlaneStatus
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
WorkView¶
-
SupportPlaneData.
WorkView
¶ Returns or sets the work view required when lock plane status is
NXOpen.GeometricUtilities.SupportPlaneDataLockPlaneStatus.AfterFirstConstraint
-------------------------------------
Getter Method
Signature
WorkView
Returns: Return type: NXOpen.View
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WorkView
Parameters: workView ( NXOpen.View
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
SupportPlaneData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.