SupportPlaneDataLockPlaneStatus Enumeration¶
NXOpen.GeometricUtilities.SupportPlaneData.LockPlaneStatus is an alias for NXOpen.GeometricUtilities.SupportPlaneDataLockPlaneStatus
-
class
NXOpen.GeometricUtilities.
SupportPlaneDataLockPlaneStatus
¶ Bases:
object
Represents support plane lock status for associative basic curves
Enum Members
Enum Member Enum Member Description No No Lock AfterFirstConstraint Lock after first constraint AfterSecondConstraint Lock after second constraint AfterThirdConstraint Lock after third constraint AfterFirstAndSecondConstraint Lock after first and second constraint AfterFirstAndThirdConstraint Lock after first and third constraint AfterSecondAndThirdConstraint Lock after second and third constraint AfterAllConstraint Lock after all constraint LockExistingPlane Lock support plane using existing face or datum CenterPointDirection Lock support plane using center point and direction, this option should be used for Center Radius Arc only -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-