PatternIncrementsBuilder Class¶
-
class
NXOpen.GeometricUtilities.
PatternIncrementsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
pattern increments builder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
IncrementsListInDirection1 | Returns the increments NXOpen.GeometricUtilities.PatternIncrementsList in Direction1. |
IncrementsListInDirection2 | Returns the increments NXOpen.GeometricUtilities.PatternIncrementsList in Direction2. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
IncrementsListInDirection1¶
-
PatternIncrementsBuilder.
IncrementsListInDirection1
¶ Returns the increments
NXOpen.GeometricUtilities.PatternIncrementsList
in Direction1.-------------------------------------
Getter Method
Signature
IncrementsListInDirection1
Returns: Return type: NXOpen.GeometricUtilities.PatternIncrementsList
New in version NX7.5.0.
License requirements: None.
IncrementsListInDirection2¶
-
PatternIncrementsBuilder.
IncrementsListInDirection2
¶ Returns the increments
NXOpen.GeometricUtilities.PatternIncrementsList
in Direction2.-------------------------------------
Getter Method
Signature
IncrementsListInDirection2
Returns: Return type: NXOpen.GeometricUtilities.PatternIncrementsList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
PatternIncrementsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.