PatternIncrementsList Class¶
-
class
NXOpen.GeometricUtilities.
PatternIncrementsList
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
list of
NXOpen.GeometricUtilities.PatternIncrementItem
objects.New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
List | Returns the list of NXOpen.GeometricUtilities.PatternIncrementItem objects. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreatePatternIncrementItem | This is the default creator for NXOpen.GeometricUtilities.PatternIncrementItem . |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
List¶
-
PatternIncrementsList.
List
¶ Returns the list of
NXOpen.GeometricUtilities.PatternIncrementItem
objects.-------------------------------------
Getter Method
Signature
List
Returns: Return type: NXOpen.GeometricUtilities.PatternIncrementItemList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
CreatePatternIncrementItem¶
-
PatternIncrementsList.
CreatePatternIncrementItem
¶ Overloaded method CreatePatternIncrementItem
CreatePatternIncrementItem()
CreatePatternIncrementItem(masterExpression)
-------------------------------------
This is the default creator for
NXOpen.GeometricUtilities.PatternIncrementItem
. Caution: This should never be called!Signature
CreatePatternIncrementItem()
Returns: Return type: NXOpen.GeometricUtilities.PatternIncrementItem
New in version NX7.5.0.
License requirements: None.
-------------------------------------
This is the actual creator for
NXOpen.GeometricUtilities.PatternIncrementItem
.Signature
CreatePatternIncrementItem(masterExpression)
Parameters: masterExpression ( NXOpen.Expression
) – the master expressionReturns: Return type: NXOpen.GeometricUtilities.PatternIncrementItem
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Validate¶
-
PatternIncrementsList.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.