OrientXpressBuilder Class¶
-
class
NXOpen.GeometricUtilities.
OrientXpressBuilder
¶ Bases:
NXOpen.TaggedObject
Represent the OrientXpress block
OrientXpress is not supported in KF.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AxisOption | Returns or sets the orientXpress active axis option |
Csys | Returns or sets the orientXpress reference csys when reference option is set to csys |
FixedCsys | Returns or sets the orientXpress fixed csys when reference option is set to fixed csys |
PlaneOption | Returns or sets the orientXpress active plane option |
ProgramDefinedCsys | Returns or sets the orientXpress program defined csys when reference option is set to program defined csys |
ReferenceOption | Returns or sets the orientXpress reference coordinate system |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
OrientXpressBuilderAxis Enumeration | the active axis option |
OrientXpressBuilderPlane Enumeration | the active plane option |
OrientXpressBuilderReference Enumeration | the option for reference csys |
Property Detail¶
AxisOption¶
-
OrientXpressBuilder.
AxisOption
¶ Returns or sets the orientXpress active axis option
-------------------------------------
Getter Method
Signature
AxisOption
Returns: Return type: NXOpen.GeometricUtilities.OrientXpressBuilderAxis
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisOption
Parameters: orientXpressAxisOption ( NXOpen.GeometricUtilities.OrientXpressBuilderAxis
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
Csys¶
-
OrientXpressBuilder.
Csys
¶ Returns or sets the orientXpress reference csys when reference option is set to csys
-------------------------------------
Getter Method
Signature
Csys
Returns: Return type: NXOpen.CoordinateSystem
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Csys
Parameters: orientXpressCsys ( NXOpen.CoordinateSystem
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
FixedCsys¶
-
OrientXpressBuilder.
FixedCsys
¶ Returns or sets the orientXpress fixed csys when reference option is set to fixed csys
-------------------------------------
Getter Method
Signature
FixedCsys
Returns: Return type: NXOpen.NXObject
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FixedCsys
Parameters: orientXpressFixedCsys ( NXOpen.NXObject
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
PlaneOption¶
-
OrientXpressBuilder.
PlaneOption
¶ Returns or sets the orientXpress active plane option
-------------------------------------
Getter Method
Signature
PlaneOption
Returns: Return type: NXOpen.GeometricUtilities.OrientXpressBuilderPlane
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlaneOption
Parameters: orientXpressPlaneOption ( NXOpen.GeometricUtilities.OrientXpressBuilderPlane
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
ProgramDefinedCsys¶
-
OrientXpressBuilder.
ProgramDefinedCsys
¶ Returns or sets the orientXpress program defined csys when reference option is set to program defined csys
-------------------------------------
Getter Method
Signature
ProgramDefinedCsys
Returns: Return type: NXOpen.NXObject
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProgramDefinedCsys
Parameters: orientXpressProgramDefinedCsys ( NXOpen.NXObject
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
ReferenceOption¶
-
OrientXpressBuilder.
ReferenceOption
¶ Returns or sets the orientXpress reference coordinate system
-------------------------------------
Getter Method
Signature
ReferenceOption
Returns: Return type: NXOpen.GeometricUtilities.OrientXpressBuilderReference
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceOption
Parameters: orientXpressReferenceOption ( NXOpen.GeometricUtilities.OrientXpressBuilderReference
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)