ModlDistanceAngle Class¶
-
class
NXOpen.GeometricUtilities.
ModlDistanceAngle
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.ModlDistanceAngle
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the value of angular transform. |
AngularDirection | Returns or sets the direction of angular dimensions. |
Distance | Returns the distance of linear transform. |
LinearAxis | Returns or sets the linear axis of distance. |
OrientXpress | Returns the orientXpress. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Angle¶
-
ModlDistanceAngle.
Angle
¶ Returns the value of angular transform.
-------------------------------------
Getter Method
Signature
Angle
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
AngularDirection¶
-
ModlDistanceAngle.
AngularDirection
¶ Returns or sets the direction of angular dimensions.
-------------------------------------
Getter Method
Signature
AngularDirection
Returns: Return type: NXOpen.Vector3d
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularDirection
Parameters: angularDirection ( NXOpen.Vector3d
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
Distance¶
-
ModlDistanceAngle.
Distance
¶ Returns the distance of linear transform.
-------------------------------------
Getter Method
Signature
Distance
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
LinearAxis¶
-
ModlDistanceAngle.
LinearAxis
¶ Returns or sets the linear axis of distance.
-------------------------------------
Getter Method
Signature
LinearAxis
Returns: Return type: NXOpen.Axis
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinearAxis
Parameters: linearAxis ( NXOpen.Axis
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
OrientXpress¶
-
ModlDistanceAngle.
OrientXpress
¶ Returns the orientXpress.
OrientXpress used as overlay in Motion.
-------------------------------------
Getter Method
Signature
OrientXpress
Returns: Return type: NXOpen.GeometricUtilities.OrientXpressBuilder
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ModlDistanceAngle.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.