ModlAlongCurveAngle Class¶
-
class
NXOpen.GeometricUtilities.
ModlAlongCurveAngle
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class
NXOpen.GeometricUtilities.ModlAlongCurveAngle
represents motion type in ModlMotionNew in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AlongCurve | Returns the value of transform. |
AlongCurveAngle | Returns the value of angular transform. |
Curve | Returns the curve on which doing the transform. |
ReverseCurveDirection | Returns or sets whether the direction of the curve to determine the transform should be reversed or not. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AlongCurve¶
-
ModlAlongCurveAngle.
AlongCurve
¶ Returns the value of transform.
-------------------------------------
Getter Method
Signature
AlongCurve
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.5.0.
License requirements: None.
AlongCurveAngle¶
-
ModlAlongCurveAngle.
AlongCurveAngle
¶ Returns the value of angular transform.
-------------------------------------
Getter Method
Signature
AlongCurveAngle
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Curve¶
-
ModlAlongCurveAngle.
Curve
¶ Returns the curve on which doing the transform.
-------------------------------------
Getter Method
Signature
Curve
Returns: Return type: NXOpen.SelectCurve
New in version NX8.5.0.
License requirements: None.
ReverseCurveDirection¶
-
ModlAlongCurveAngle.
ReverseCurveDirection
¶ Returns or sets whether the direction of the curve to determine the transform should be reversed or not.
-------------------------------------
Getter Method
Signature
ReverseCurveDirection
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseCurveDirection
Parameters: reverseCurveDirection (bool) – New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ModlAlongCurveAngle.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.