FtmTransformCurvesBuilder Class¶
-
class
NXOpen.GeometricUtilities.
FtmTransformCurvesBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricUtilities.FtmTransformCurvesBuilder
builderTo create a new instance of this class, use
NXOpen.GeometricUtilities.OmnicadManager.CreateFtmTransformCurvesBuilder()
Default values.
Property Value AlignBreakPoints 0 OppositeSense 0 OppositeSide 0 TransformCurvesContinuity G0 TransformCurvesMagnitude.Value 1 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AlignBreakPoints | Returns or sets the option for aligning break points used in the transformation or morphing calculations |
OppositeSense | Returns or sets the option to reverse the OmniCAD pre-determined direction for the transformation start and end curves |
OppositeSide | Returns or sets the option to change the displacements to the opposite side of the transformation |
Tag | Returns the Tag for this object. |
TransformCurvesContinuity | Returns or sets the continuity option for the transformation start and end curves used in the transformation or morphing calculations |
TransformCurvesMagnitude | Returns the magnitude controlled by continuity for the transformation curves |
TransformEndCurves | Returns the end or target constraint for the product shape in the form of curves used in the transformation or morphing calculations |
TransformStartCurves | Returns the starting constraint for the product shape in the form of curves used in the transformation or morphing calculations |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FtmTransformCurvesBuilderTransformCurvesContinuityType Enumeration | Transform curves continuity type |
Property Detail¶
AlignBreakPoints¶
-
FtmTransformCurvesBuilder.
AlignBreakPoints
¶ Returns or sets the option for aligning break points used in the transformation or morphing calculations
-------------------------------------
Getter Method
Signature
AlignBreakPoints
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignBreakPoints
Parameters: alignBreakPoints (bool) – New in version NX10.0.0.
License requirements: None.
OppositeSense¶
-
FtmTransformCurvesBuilder.
OppositeSense
¶ Returns or sets the option to reverse the OmniCAD pre-determined direction for the transformation start and end curves
-------------------------------------
Getter Method
Signature
OppositeSense
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OppositeSense
Parameters: oppositeSense (bool) – New in version NX10.0.0.
License requirements: None.
OppositeSide¶
-
FtmTransformCurvesBuilder.
OppositeSide
¶ Returns or sets the option to change the displacements to the opposite side of the transformation
-------------------------------------
Getter Method
Signature
OppositeSide
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OppositeSide
Parameters: oppositeSide (bool) – New in version NX10.0.0.
License requirements: None.
TransformCurvesContinuity¶
-
FtmTransformCurvesBuilder.
TransformCurvesContinuity
¶ Returns or sets the continuity option for the transformation start and end curves used in the transformation or morphing calculations
-------------------------------------
Getter Method
Signature
TransformCurvesContinuity
Returns: Return type: NXOpen.GeometricUtilities.FtmTransformCurvesBuilderTransformCurvesContinuityType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransformCurvesContinuity
Parameters: transformCurvesContinuity ( NXOpen.GeometricUtilities.FtmTransformCurvesBuilderTransformCurvesContinuityType
) –New in version NX10.0.0.
License requirements: None.
TransformCurvesMagnitude¶
-
FtmTransformCurvesBuilder.
TransformCurvesMagnitude
¶ Returns the magnitude controlled by continuity for the transformation curves
-------------------------------------
Getter Method
Signature
TransformCurvesMagnitude
Returns: Return type: NXOpen.Expression
New in version NX11.0.1.
License requirements: None.
TransformEndCurves¶
-
FtmTransformCurvesBuilder.
TransformEndCurves
¶ Returns the end or target constraint for the product shape in the form of curves used in the transformation or morphing calculations
-------------------------------------
Getter Method
Signature
TransformEndCurves
Returns: Return type: NXOpen.Section
New in version NX10.0.0.
License requirements: None.
TransformStartCurves¶
-
FtmTransformCurvesBuilder.
TransformStartCurves
¶ Returns the starting constraint for the product shape in the form of curves used in the transformation or morphing calculations
-------------------------------------
Getter Method
Signature
TransformStartCurves
Returns: Return type: NXOpen.Section
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
FtmTransformCurvesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.