FtmTransformCurvesBuilderTransformCurvesContinuityType Enumeration

NXOpen.GeometricUtilities.FtmTransformCurvesBuilder.TransformCurvesContinuityType is an alias for NXOpen.GeometricUtilities.FtmTransformCurvesBuilderTransformCurvesContinuityType

class NXOpen.GeometricUtilities.FtmTransformCurvesBuilderTransformCurvesContinuityType

Bases: object

Transform curves continuity type

Enum Members

Enum Member Enum Member Description
G0
G1
G2
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.