FaceSetDataCollection Class

class NXOpen.GeometricUtilities.FaceSetDataCollection

Bases: object

This class contains the factory methods for creating an FaceSetData.

To obtain an instance of this class, refer to NXOpen.Part

New in version NX5.0.0.

Deprecated since version NX8.5.0: This class is never used and can be safely removed

Methods

Method Description
Create Creates an FaceSetData.

Method Detail

Create

FaceSetDataCollection.Create

Creates an FaceSetData.

Signature Create(mFaceCollector, mReverseNormalFlag)

Parameters:
  • mFaceCollector (NXOpen.ScCollector) – the face set collector
  • mReverseNormalFlag (bool) – the face set reverse direction flag
Returns:

Return type:

NXOpen.GeometricUtilities.FaceSetData

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)