BlendStopshortBuilderCollection Class

class NXOpen.GeometricUtilities.BlendStopshortBuilderCollection

Bases: object

This class contains the factory methods for creating an BlendStopshortBuilder.

To obtain an instance of this class, refer to NXOpen.Part

New in version NX5.0.0.

Methods

Method Description
Create Creates an BlendStopshortBuilder.

Method Detail

Create

BlendStopshortBuilderCollection.Create

Creates an BlendStopshortBuilder.

Signature Create(mChoice, mOnPathExp, mPath, mIsFlipped, mThruPoint)

Parameters:
Returns:

Return type:

NXOpen.GeometricUtilities.BlendStopshortBuilder

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)