BlendStopshortBuilder Class¶
-
class
NXOpen.GeometricUtilities.
BlendStopshortBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.BlendStopshortBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Choice | Returns or sets the Stopshort option choice. |
OnPath | Returns the NXOpen.GeometricUtilities.BlendStopshortBuilder subobject. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Destroy | Destructor for NXOpen.GeometricUtilities.BlendStopshortBuilder |
FlipPath | Flip the builder path for NXOpen.GeometricUtilities.BlendStopshortBuilder |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BlendStopshortBuilderChoices Enumeration | This enum represents the choice for stopshort option. |
Property Detail¶
Choice¶
-
BlendStopshortBuilder.
Choice
¶ Returns or sets the Stopshort option choice.
Choose from ‘At Distance’ or ‘At Intersection’.
-------------------------------------
Getter Method
Signature
Choice
Returns: Return type: NXOpen.GeometricUtilities.BlendStopshortBuilderChoices
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Choice
Parameters: mChoice ( NXOpen.GeometricUtilities.BlendStopshortBuilderChoices
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OnPath¶
-
BlendStopshortBuilder.
OnPath
¶ Returns the
NXOpen.GeometricUtilities.BlendStopshortBuilder
subobject.-------------------------------------
Getter Method
Signature
OnPath
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Destroy¶
-
BlendStopshortBuilder.
Destroy
¶ Destructor for
NXOpen.GeometricUtilities.BlendStopshortBuilder
Signature
Destroy()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FlipPath¶
-
BlendStopshortBuilder.
FlipPath
¶ Flip the builder path for
NXOpen.GeometricUtilities.BlendStopshortBuilder
Signature
FlipPath()
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
BlendStopshortBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.