AngularPatternSpacing Class¶
-
class
NXOpen.GeometricUtilities.
AngularPatternSpacing
¶ Bases:
NXOpen.GeometricUtilities.PatternSpacing
defines the various ways pattern instances can be spaced within the pattern, particularly in the context of the PatternDefinition class.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
NCopies | Returns the number of copies the pattern will generated in this direction |
PitchAngle | Returns the angle for the spacing of the pattern from one instance to the next. |
PitchDistance | Returns the circumfrential distance for the spacing of the pattern from one instance to the next. |
SpaceType | Returns or sets the type of spacing to be used by the pattern |
SpacingsList | Returns the list of spacings (Expression or OnPathDimBuilder) to be used in this direction |
SpanAngle | Returns the angle for the spacing of the pattern for the entire pattern. |
Tag | Returns the Tag for this object. |
UsePitchOption | Returns or sets the switch to use Pitch Distance or Pitch Angle. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AngularPatternSpacingUsePitchOptions Enumeration | This defines Use Pitch As options |
Property Detail¶
PitchAngle¶
-
AngularPatternSpacing.
PitchAngle
¶ Returns the angle for the spacing of the pattern from one instance to the next.
-------------------------------------
Getter Method
Signature
PitchAngle
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
PitchDistance¶
-
AngularPatternSpacing.
PitchDistance
¶ Returns the circumfrential distance for the spacing of the pattern from one instance to the next.
-------------------------------------
Getter Method
Signature
PitchDistance
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
SpanAngle¶
-
AngularPatternSpacing.
SpanAngle
¶ Returns the angle for the spacing of the pattern for the entire pattern.
-------------------------------------
Getter Method
Signature
SpanAngle
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
UsePitchOption¶
-
AngularPatternSpacing.
UsePitchOption
¶ Returns or sets the switch to use Pitch Distance or Pitch Angle.
-------------------------------------
Getter Method
Signature
UsePitchOption
Returns: Return type: NXOpen.GeometricUtilities.AngularPatternSpacingUsePitchOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UsePitchOption
Parameters: usePitchOption ( NXOpen.GeometricUtilities.AngularPatternSpacingUsePitchOptions
) –New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
AngularPatternSpacing.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.