AngularPatternSpacingUsePitchOptions Enumeration¶
NXOpen.GeometricUtilities.AngularPatternSpacing.UsePitchOptions is an alias for NXOpen.GeometricUtilities.AngularPatternSpacingUsePitchOptions
-
class
NXOpen.GeometricUtilities.
AngularPatternSpacingUsePitchOptions
¶ Bases:
object
This defines Use Pitch As options
Enum Members
Enum Member Enum Member Description Angle angle is pitch value Distance distance is pitch value. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-