HighlightLinesAnalysisBuilder Class¶
-
class
NXOpen.GeometricAnalysis.
HighlightLinesAnalysisBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricAnalysis.HighlightLinesAnalysis
builder.Highlight Lines Analysis function can produce both reflection lines and projection lines which are used to evaluate the surface quality and continuity between adjacent surfaces.
To create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisObjectCollection.CreateHighlightLinesAnalysisBuilder()
Default values.
Property Value EndIsoAngle.Value 90 LightNumber 10 LightSpacing 50.0 (millimeters part), 2.0 (inches part) Resolution Fine StartIsoAngle.Value -90 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BetweenPoints | Returns the between points |
DisplayMethod | Returns or sets the display method |
EndIsoAngle | Returns the end angle for isoclines (uniform) |
Faces | Returns the face list |
IsReflectionLocked | Returns or sets the lock reflection. |
IsoclineVector | Returns or sets the vector to define isoclines |
LightDiffuseness | Returns or sets the ratio of blended texels to all light texels. |
LightNumber | Returns or sets the number of lights. |
LightPlacement | Returns or sets the light placement |
LightPlaneOrigin | Returns the origin of the light plane |
LightPlaneXAxis | Returns the x-axis of the light plane |
LightPlaneYAxis | Returns the y-axis of the light plane |
LightSpacing | Returns or sets the light spacing between two adjacent lights. |
LightWidth | Returns or sets the ratio of light size to light spacing. |
Resolution | Returns or sets the resolution. |
StartIsoAngle | Returns the start angle for isoclines (uniform) |
Tag | Returns the Tag for this object. |
ThroughPoints | Returns the through points |
Type | Returns or sets the type |
Type2 | Returns or sets the display type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetBrightColor | Gets the color of the bright (lit) areas of reflection contours |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDarkColor | Gets the color of the dark (unlit) areas of reflection contours |
GetObject | Returns the object currently being edited by this builder. |
ReinitializePlane | Reinitialize light plane based on the selected faces. |
SetBrightColor | Sets the color of the bright (lit) areas of reflection contours |
SetDarkColor | Sets the color of the dark (unlit) areas of reflection contours |
SetLightPlaneOrigin | Sets the origin of the light plane. |
SetLightPlaneXAxis | Sets the x-axis of the light plane. |
SetLightPlaneYAxis | Sets the y-axis of the light plane. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HighlightLinesAnalysisBuilderDisplayMethods Enumeration | display methods |
HighlightLinesAnalysisBuilderLightPlacements Enumeration | light placement |
HighlightLinesAnalysisBuilderLightPlaneOptions Enumeration | light plane options |
HighlightLinesAnalysisBuilderResolutions Enumeration | resolution options |
HighlightLinesAnalysisBuilderTypes Enumeration | three types of light methods |
HighlightLinesAnalysisBuilderTypes2 Enumeration | four types of display methods |
Property Detail¶
BetweenPoints¶
-
HighlightLinesAnalysisBuilder.
BetweenPoints
¶ Returns the between points
-------------------------------------
Getter Method
Signature
BetweenPoints
Returns: Return type: NXOpen.SelectPointList
New in version NX6.0.0.
License requirements: None.
DisplayMethod¶
-
HighlightLinesAnalysisBuilder.
DisplayMethod
¶ Returns or sets the display method
-------------------------------------
Getter Method
Signature
DisplayMethod
Returns: Return type: NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderDisplayMethods
New in version NX6.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilder.Type2`()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayMethod
Parameters: displayMethod ( NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderDisplayMethods
) –New in version NX6.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilder.Type2`()
instead.License requirements: studio_analyze (“STUDIO ANALYZE”)
EndIsoAngle¶
-
HighlightLinesAnalysisBuilder.
EndIsoAngle
¶ Returns the end angle for isoclines (uniform)
-------------------------------------
Getter Method
Signature
EndIsoAngle
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Faces¶
-
HighlightLinesAnalysisBuilder.
Faces
¶ Returns the face list
-------------------------------------
Getter Method
Signature
Faces
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX6.0.0.
License requirements: None.
IsReflectionLocked¶
-
HighlightLinesAnalysisBuilder.
IsReflectionLocked
¶ Returns or sets the lock reflection.
When the lock is on, the reflection lines will be freezed while the view is changing. Otherwise, the reflection lines will be updated continuously while view is changing.
-------------------------------------
Getter Method
Signature
IsReflectionLocked
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsReflectionLocked
Parameters: isReflectionLocked (bool) – New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
IsoclineVector¶
-
HighlightLinesAnalysisBuilder.
IsoclineVector
¶ Returns or sets the vector to define isoclines
-------------------------------------
Getter Method
Signature
IsoclineVector
Returns: Return type: NXOpen.Direction
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsoclineVector
Parameters: isoclineVector ( NXOpen.Direction
) –New in version NX8.5.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
LightDiffuseness¶
-
HighlightLinesAnalysisBuilder.
LightDiffuseness
¶ Returns or sets the ratio of blended texels to all light texels.
It is used by reflection contours
-------------------------------------
Getter Method
Signature
LightDiffuseness
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LightDiffuseness
Parameters: lightDiffuseness (float) – New in version NX9.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
LightNumber¶
-
HighlightLinesAnalysisBuilder.
LightNumber
¶ Returns or sets the number of lights.
It’s used by Uniform type and Between Points type.
-------------------------------------
Getter Method
Signature
LightNumber
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LightNumber
Parameters: lightNumber (int) – New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
LightPlacement¶
-
HighlightLinesAnalysisBuilder.
LightPlacement
¶ Returns or sets the light placement
-------------------------------------
Getter Method
Signature
LightPlacement
Returns: Return type: NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderLightPlacements
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LightPlacement
Parameters: placement ( NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderLightPlacements
) –New in version NX8.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
LightPlaneOrigin¶
-
HighlightLinesAnalysisBuilder.
LightPlaneOrigin
¶ Returns the origin of the light plane
-------------------------------------
Getter Method
Signature
LightPlaneOrigin
Returns: coordinates of origin Return type: NXOpen.Point3d
New in version NX6.0.0.
License requirements: None.
LightPlaneXAxis¶
-
HighlightLinesAnalysisBuilder.
LightPlaneXAxis
¶ Returns the x-axis of the light plane
-------------------------------------
Getter Method
Signature
LightPlaneXAxis
Returns: x-axis vector Return type: NXOpen.Vector3d
New in version NX6.0.0.
License requirements: None.
LightPlaneYAxis¶
-
HighlightLinesAnalysisBuilder.
LightPlaneYAxis
¶ Returns the y-axis of the light plane
-------------------------------------
Getter Method
Signature
LightPlaneYAxis
Returns: y-axis vector Return type: NXOpen.Vector3d
New in version NX6.0.0.
License requirements: None.
LightSpacing¶
-
HighlightLinesAnalysisBuilder.
LightSpacing
¶ Returns or sets the light spacing between two adjacent lights.
It’s used by Uniform type
-------------------------------------
Getter Method
Signature
LightSpacing
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LightSpacing
Parameters: lightSpacing (float) – New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
LightWidth¶
-
HighlightLinesAnalysisBuilder.
LightWidth
¶ Returns or sets the ratio of light size to light spacing.
It is used by reflection contours
-------------------------------------
Getter Method
Signature
LightWidth
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LightWidth
Parameters: lightWidth (float) – New in version NX9.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Resolution¶
-
HighlightLinesAnalysisBuilder.
Resolution
¶ Returns or sets the resolution.
-------------------------------------
Getter Method
Signature
Resolution
Returns: Return type: NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderResolutions
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Resolution
Parameters: resolution ( NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderResolutions
) –New in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
StartIsoAngle¶
-
HighlightLinesAnalysisBuilder.
StartIsoAngle
¶ Returns the start angle for isoclines (uniform)
-------------------------------------
Getter Method
Signature
StartIsoAngle
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
ThroughPoints¶
-
HighlightLinesAnalysisBuilder.
ThroughPoints
¶ Returns the through points
-------------------------------------
Getter Method
Signature
ThroughPoints
Returns: Return type: NXOpen.SelectPointList
New in version NX6.0.0.
License requirements: None.
Type¶
-
HighlightLinesAnalysisBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderTypes
New in version NX6.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilder.LightPlacement`()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderTypes
) –New in version NX6.0.0.
Deprecated since version NX8.0.0: Use
NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilder.LightPlacement`()
instead.License requirements: studio_analyze (“STUDIO ANALYZE”)
Type2¶
-
HighlightLinesAnalysisBuilder.
Type2
¶ Returns or sets the display type
-------------------------------------
Getter Method
Signature
Type2
Returns: Return type: NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderTypes2
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type2
Parameters: type ( NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderTypes2
) –New in version NX8.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Method Detail¶
GetBrightColor¶
-
HighlightLinesAnalysisBuilder.
GetBrightColor
¶ Gets the color of the bright (lit) areas of reflection contours
Signature
GetBrightColor()
Returns: Array of 3 RGB values, each between 0 and 1 Return type: list of float New in version NX9.0.0.
License requirements: None.
GetDarkColor¶
-
HighlightLinesAnalysisBuilder.
GetDarkColor
¶ Gets the color of the dark (unlit) areas of reflection contours
Signature
GetDarkColor()
Returns: Array of 3 RGB values, each between 0 and 1 Return type: list of float New in version NX9.0.0.
License requirements: None.
ReinitializePlane¶
-
HighlightLinesAnalysisBuilder.
ReinitializePlane
¶ Reinitialize light plane based on the selected faces.
If more faces are selected, you may need to change light plane, so the light plane could be better centered.
Signature
ReinitializePlane()
New in version NX6.0.0.
Deprecated since version NX8.0.0: This call currently does not do anything. Calls to this method can be safely removed.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SetBrightColor¶
-
HighlightLinesAnalysisBuilder.
SetBrightColor
¶ Sets the color of the bright (lit) areas of reflection contours
Signature
SetBrightColor(brightColor)
Parameters: brightColor (list of float) – Array of 3 RGB values, each between 0 and 1 New in version NX9.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SetDarkColor¶
-
HighlightLinesAnalysisBuilder.
SetDarkColor
¶ Sets the color of the dark (unlit) areas of reflection contours
Signature
SetDarkColor(darkColor)
Parameters: darkColor (list of float) – Array of 3 RGB values, each between 0 and 1 New in version NX9.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SetLightPlaneOrigin¶
-
HighlightLinesAnalysisBuilder.
SetLightPlaneOrigin
¶ Sets the origin of the light plane.
Signature
SetLightPlaneOrigin(origin)
Parameters: origin ( NXOpen.Point3d
) – coordinates of originNew in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SetLightPlaneXAxis¶
-
HighlightLinesAnalysisBuilder.
SetLightPlaneXAxis
¶ Sets the x-axis of the light plane.
Signature
SetLightPlaneXAxis(xAxis)
Parameters: xAxis ( NXOpen.Vector3d
) – x-axis vectorNew in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
SetLightPlaneYAxis¶
-
HighlightLinesAnalysisBuilder.
SetLightPlaneYAxis
¶ Sets the y-axis of the light plane.
Signature
SetLightPlaneYAxis(yAxis)
Parameters: yAxis ( NXOpen.Vector3d
) – y-axis vectorNew in version NX6.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
Validate¶
-
HighlightLinesAnalysisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.