HighlightLinesAnalysisBuilderResolutions Enumeration¶
NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilder.Resolutions is an alias for NXOpen.GeometricAnalysis.HighlightLinesAnalysisBuilderResolutions
-
class
NXOpen.GeometricAnalysis.
HighlightLinesAnalysisBuilderResolutions
¶ Bases:
object
resolution options
Enum Members
Enum Member Enum Member Description Coarse Coarse Standard Standard Fine Fine ExtraFine Extra Fine SuperFine Super Fine UltraFine Ultra Fine -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-