SpatialMapTypeEnum Enumeration¶
NXOpen.Fields.SpatialMap.TypeEnum is an alias for NXOpen.Fields.SpatialMapTypeEnum
-
class
NXOpen.Fields.
SpatialMapTypeEnum
¶ Bases:
object
Type of Spatial Map
Enum Members
Enum Member Enum Member Description NotSet No Map Global Map to global csys - defaults to cartesian Cartesian Map to cartesian csys Cylindrical Map to cylindrical csys Spherical Map to spherical csys ParametricSpace Map to parametric space - see NXOpen.Fields.SpatialMapBoundingBoxMapEnum
ParametricPlane Map to parametric plane - see NXOpen.Fields.SpatialMapParametricPlaneMapEnum
ParametricLine Map to parametric line ImportedParametricLine map to imported parametric line -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-