SpatialMapBoundingBoxMapEnum Enumeration

NXOpen.Fields.SpatialMap.BoundingBoxMapEnum is an alias for NXOpen.Fields.SpatialMapBoundingBoxMapEnum

class NXOpen.Fields.SpatialMapBoundingBoxMapEnum

Bases: object

Bounding Box Map

Enum Members

Enum Member Enum Member Description
OppositeCorner
Objects
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.