FieldFormula Class¶
-
class
NXOpen.Fields.
FieldFormula
¶ Bases:
NXOpen.Fields.Field
Represents the Field Formula class.
A field (see
NXOpen.Fields.Field
) which has **<tt>n</tt></b> number of dependent variables, where each dependent variable (seeNXOpen.Fields.FieldVariable
) is implemented using the NX Expression sub-system. In practical terms, a field formula is implemented using n number of field expressionsNXOpen.Fields.FieldExpression
.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
IsBlanked | Returns the blank status of this object. |
IsLocked | Returns a value that indicates whether this field is locked against edits. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsUserField | Returns a value that indicates whether this field is a user created/managed field. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddApplicationData | Adds the specified application data object to the field NOTE: Only one application data object per IApplication can be added and the data must be owned by an IApplication with the same Part::Field::Main as the field. |
Blank | Blanks the object. |
CopyAsTableToPart | Create a new table field from this field (regardless of type). |
CopyToPart | Copy the field to the target part. |
CreateAttributeIterator | Create an attribute iterator |
CreateCopyInPart | Copy the field to the target part. |
CreateDrawHelper | Creates a field drawhelper which can be used to get display attributes of this field. |
CreateTableInPart | Create a new table field from this field (regardless of type). |
Delete | Delete this field; destroys the field and removes all references to it. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
EditFieldFormula | Edit the formula field. |
EditFieldFormulaVariables | Edit the formula field variables. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetApplicationData | Retrieves the application data associated with the field for the specified application. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDependentExpressions | Returns the dependent field expressions associated with this formula |
GetDependentVariables | Returns the dependent variables for this NXOpen.Fields.Field |
GetDescription | Returns the description of the field. |
GetFieldDrawhelper | Returns a field drawhelper which can be used to get display attributes of this field. |
GetFieldEvaluator | Returns a field evaluator which can be used to evaluate this field. |
GetIdLabel | Returns the ID/Label of the field. |
GetIndependentVariables | Returns the independent variables for this NXOpen.Fields.Field |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSpatialMap | Returns the spatial map for the formula field if one exists. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Highlight | Highlights the object. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveViewDependency | Remove dependency on all views from an object. |
Rename | Update the name of the field. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDescription | Update the description of the field. |
SetIdLabel | Update the ID/Label of the field. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetPartContext | Set part context. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSpatialMap | Set the spatial map for the formula field. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
XYGraph | Creates displayed graphs of the Field’s specified independent variable versus all the Field’s dependent variables |
XYGraph3D | Plots or overlays graphs of the Field’s specified x-axis and z-axis independent variables versus the Field’s specified y-axis dependent variable ; returns newly created plot object. |
XYGraphArgand | Plots the Field’s specified independent variable versus all the Field’s scaled dependent variables as an Argand graph; returns newly created plot object(s). |
Property Detail¶
IsOccurrence¶
-
FieldFormula.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
FieldFormula.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
FieldFormula.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
FieldFormula.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
FieldFormula.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
FieldFormula.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
EditFieldFormula¶
-
FieldFormula.
EditFieldFormula
¶ Edit the formula field.
Specifies the new expression
NXOpen.Fields.FieldExpression
array and the array of :py:class:`NXOpen.Fields.FieldVariable`s used.Signature
EditFieldFormula(indepVarArray, depExpArray)
Parameters: - indepVarArray (list of
NXOpen.Fields.FieldVariable
) – independent variables to be associated with the field - depExpArray (list of
NXOpen.Fields.FieldExpression
) – dependent field expressions to be associated with the field
New in version NX6.0.0.
License requirements: None.
- indepVarArray (list of
EditFieldFormulaVariables¶
-
FieldFormula.
EditFieldFormulaVariables
¶ Edit the formula field variables.
Specifies the new dependent and independent
NXOpen.Fields.FieldVariable
arrays. The formula will be updated to reflect the changes (if any) to the variables. If the dependent variables are changed, the expressions will be changed to 0 if the new variable measure is incompatible with the old variable measure. If the independent variables change, the expression will be changed to 0 if it contains any of the deleted variables.Signature
EditFieldFormulaVariables(indepVarArray, depVarArray)
Parameters: - indepVarArray (list of
NXOpen.Fields.FieldVariable
) – new independent variables to be associated with the field - depVarArray (list of
NXOpen.Fields.FieldVariable
) – new dependent field variables to be associated with the field
New in version NX12.0.0.
License requirements: None.
- indepVarArray (list of
FindObject¶
-
FieldFormula.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetDependentExpressions¶
-
FieldFormula.
GetDependentExpressions
¶ Returns the dependent field expressions associated with this formula
Signature
GetDependentExpressions()
Returns: dependent expressions Return type: list of NXOpen.Fields.FieldExpression
New in version NX11.0.0.
License requirements: None.
Print¶
-
FieldFormula.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
FieldFormula.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.