HeadImpactRPillarWizardBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
HeadImpactRPillarWizardBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.VehicleDesign.HeadImpactRPillarWizardBuilder
.This is an abstract class and cannot be instantiated.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
RP2Left | Returns or sets the left rear pillar 2 point. |
RP2Right | Returns or sets the right rear pillar 2 point. |
RPillarLeft | Returns the left rear pillar geometry. |
RPillarRight | Returns the right rear pillar geometry. |
Tag | Returns the Tag for this object. |
UpperRoofInterior | Returns the upper roof interior geometry. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
RP2Left¶
-
HeadImpactRPillarWizardBuilder.
RP2Left
¶ Returns or sets the left rear pillar 2 point.
-------------------------------------
Getter Method
Signature
RP2Left
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RP2Left
Parameters: rp2Left ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RP2Right¶
-
HeadImpactRPillarWizardBuilder.
RP2Right
¶ Returns or sets the right rear pillar 2 point.
-------------------------------------
Getter Method
Signature
RP2Right
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RP2Right
Parameters: rp2Right ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RPillarLeft¶
-
HeadImpactRPillarWizardBuilder.
RPillarLeft
¶ Returns the left rear pillar geometry.
-------------------------------------
Getter Method
Signature
RPillarLeft
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
RPillarRight¶
-
HeadImpactRPillarWizardBuilder.
RPillarRight
¶ Returns the right rear pillar geometry.
-------------------------------------
Getter Method
Signature
RPillarRight
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
UpperRoofInterior¶
-
HeadImpactRPillarWizardBuilder.
UpperRoofInterior
¶ Returns the upper roof interior geometry.
-------------------------------------
Getter Method
Signature
UpperRoofInterior
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
HeadImpactRPillarWizardBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.