BaseDataSourceBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
BaseDataSourceBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.VehicleDesign.BaseDataSourceBuilder
builder, which set the base data source for work part in assembly context.To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateBaseDataSourceBuilder()
New in version NX11.0.1.
Properties¶
Property | Description |
---|---|
BaseDataSource | Returns the base data source for work part. |
BaseDataSourceMethod | Returns or sets the base data source option, the component selected or display part should contain Base Data feature group |
DelayUpdate | Returns or sets the method to set update delay option between assembly components. |
RemoveBaseDataAttr | Returns or sets the method to remove Base Data attribute of work part, it is a locked attribute. |
RemoveBaseDataSourceAttr | Returns or sets the method to remove Base Data Source attribute of work part, it is a locked attribute. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BaseDataSourceBuilderBaseDataSourceOption Enumeration | Represents the base data source option, you can select one component or display part which contains the Base Data feature group for current work part. |
Property Detail¶
BaseDataSource¶
-
BaseDataSourceBuilder.
BaseDataSource
¶ Returns the base data source for work part.
This is effective for select component method.
-------------------------------------
Getter Method
Signature
BaseDataSource
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX11.0.1.
License requirements: None.
BaseDataSourceMethod¶
-
BaseDataSourceBuilder.
BaseDataSourceMethod
¶ Returns or sets the base data source option, the component selected or display part should contain Base Data feature group
-------------------------------------
Getter Method
Signature
BaseDataSourceMethod
Returns: Return type: NXOpen.Features.VehicleDesign.BaseDataSourceBuilderBaseDataSourceOption
New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BaseDataSourceMethod
Parameters: baseDataSourceOption ( NXOpen.Features.VehicleDesign.BaseDataSourceBuilderBaseDataSourceOption
) –New in version NX11.0.1.
License requirements: nx_general_packaging (“NX General Packaging”)
DelayUpdate¶
-
BaseDataSourceBuilder.
DelayUpdate
¶ Returns or sets the method to set update delay option between assembly components.
-------------------------------------
Getter Method
Signature
DelayUpdate
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
DelayUpdate
Parameters: delayUpdate (bool) – New in version NX11.0.1.
License requirements: nx_general_packaging (“NX General Packaging”)
RemoveBaseDataAttr¶
-
BaseDataSourceBuilder.
RemoveBaseDataAttr
¶ Returns or sets the method to remove Base Data attribute of work part, it is a locked attribute.
-------------------------------------
Getter Method
Signature
RemoveBaseDataAttr
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
RemoveBaseDataAttr
Parameters: removeBaseDataAttr (bool) – New in version NX11.0.1.
License requirements: nx_general_packaging (“NX General Packaging”)
RemoveBaseDataSourceAttr¶
-
BaseDataSourceBuilder.
RemoveBaseDataSourceAttr
¶ Returns or sets the method to remove Base Data Source attribute of work part, it is a locked attribute.
-------------------------------------
Getter Method
Signature
RemoveBaseDataSourceAttr
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
RemoveBaseDataSourceAttr
Parameters: removeBaseDataSourceAttr (bool) – New in version NX11.0.1.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
BaseDataSourceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.