BaseDataSourceBuilderBaseDataSourceOption Enumeration¶
NXOpen.Features.VehicleDesign.BaseDataSourceBuilder.BaseDataSourceOption is an alias for NXOpen.Features.VehicleDesign.BaseDataSourceBuilderBaseDataSourceOption
-
class
NXOpen.Features.VehicleDesign.
BaseDataSourceBuilderBaseDataSourceOption
¶ Bases:
object
Represents the base data source option, you can select one component or display part which contains the Base Data feature group for current work part.
Enum Members
Enum Member Enum Member Description SelectComponent Component which contains Base Data feature group. DisplayPart -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-