TubeBuilder Class¶
-
class
NXOpen.Features.
TubeBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.Tube
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateTubeBuilder()
Default values.
Property Value BooleanOption.Type Create InnerDiameter.Value 0 (millimeters part), 0 (inches part) OuterDiameter.Value 1 (millimeters part), 0.04 (inches part) OutputOption MultipleSegments New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BooleanOption | Returns the boolean option |
InnerDiameter | Returns the inner diameter |
OuterDiameter | Returns the outer diameter |
OutputOption | Returns or sets the output topology option |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PathSection | Returns the path section |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the distance tolerance |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TubeBuilderOutput Enumeration | This enum represents the topology output option |
Property Detail¶
BooleanOption¶
-
TubeBuilder.
BooleanOption
¶ Returns the boolean option
-------------------------------------
Getter Method
Signature
BooleanOption
Returns: Return type: NXOpen.GeometricUtilities.BooleanOperation
New in version NX5.0.0.
License requirements: None.
InnerDiameter¶
-
TubeBuilder.
InnerDiameter
¶ Returns the inner diameter
-------------------------------------
Getter Method
Signature
InnerDiameter
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
OuterDiameter¶
-
TubeBuilder.
OuterDiameter
¶ Returns the outer diameter
-------------------------------------
Getter Method
Signature
OuterDiameter
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
OutputOption¶
-
TubeBuilder.
OutputOption
¶ Returns or sets the output topology option
-------------------------------------
Getter Method
Signature
OutputOption
Returns: Return type: NXOpen.Features.TubeBuilderOutput
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputOption
Parameters: outputOption ( NXOpen.Features.TubeBuilderOutput
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PathSection¶
-
TubeBuilder.
PathSection
¶ Returns the path section
-------------------------------------
Getter Method
Signature
PathSection
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: None.
Tolerance¶
-
TubeBuilder.
Tolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: tolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
TubeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.