ToolingCollection Class¶
-
class
NXOpen.Features.
ToolingCollection
¶ Bases:
object
This class contains the factory method for creating tooling feature builder.
To obtain an instance of this class, refer to
NXOpen.Features.FeatureCollection
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CreatePrebendBuilder | Creates a NXOpen.Tooling.PrebendBuilder |
CreateUniversalUnformBuilder | Creates a NXOpen.Tooling.UniversalUnformBuilder |
ToolingFindObject | Finds the NXOpen.Features with the given identifier as recorded in a journal. |
Method Detail¶
CreatePrebendBuilder¶
-
ToolingCollection.
CreatePrebendBuilder
¶ Creates a
NXOpen.Tooling.PrebendBuilder
Signature
CreatePrebendBuilder(prebend)
Parameters: prebend ( NXOpen.Features.Prebend
) –NXOpen.Features.Prebend
to be editedReturns: PrebendBuilder object Return type: NXOpen.Tooling.PrebendBuilder
New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
CreateUniversalUnformBuilder¶
-
ToolingCollection.
CreateUniversalUnformBuilder
¶ Creates a
NXOpen.Tooling.UniversalUnformBuilder
Signature
CreateUniversalUnformBuilder(universalUnform)
Parameters: universalUnform ( NXOpen.Features.UniversalUnform
) –NXOpen.Features.UniversalUnform
to be editedReturns: UniversalUnformBuilder object Return type: NXOpen.Tooling.UniversalUnformBuilder
New in version NX8.5.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ToolingFindObject¶
-
ToolingCollection.
ToolingFindObject
¶ Finds the
NXOpen.Features
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
ToolingFindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Feature with this identifier Return type: NXOpen.Features.Feature
New in version NX8.5.0.
License requirements: None.