SubdivisionRevolveBuilder Class¶
-
class
NXOpen.Features.Subdivision.
SubdivisionRevolveBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.Subdivision.SubdivisionRevolveBuilder
builder.To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateSubdivisionRevolveBuilder()
Default values.
Property Value CanSew 1 EndAngle.Value 360 NumOfSegments 8 StartAngle.Value 0 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AxisPoint | Returns the origin of the axis of revolution. |
AxisVector | Returns or sets the axis of revolution. |
CanSew | Returns or sets the value indicating if open edges of the revolve mesh can be sewn with selected input open edges. |
Continuity | Returns or sets the continuity. |
EndAngle | Returns the end of angular dimension. |
NumOfSegments | Returns or sets the number of segments. |
SectionObject | Returns the section as revolving profile. |
StartAngle | Returns the start of angular dimension. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SubdivisionRevolveBuilderContinuityType Enumeration | Type of continuity. |
Property Detail¶
AxisPoint¶
-
SubdivisionRevolveBuilder.
AxisPoint
¶ Returns the origin of the axis of revolution.
-------------------------------------
Getter Method
Signature
AxisPoint
Returns: Return type: NXOpen.SelectNXObject
New in version NX10.0.0.
License requirements: None.
AxisVector¶
-
SubdivisionRevolveBuilder.
AxisVector
¶ Returns or sets the axis of revolution.
-------------------------------------
Getter Method
Signature
AxisVector
Returns: Return type: NXOpen.Direction
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisVector
Parameters: axisVector ( NXOpen.Direction
) –New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
CanSew¶
-
SubdivisionRevolveBuilder.
CanSew
¶ Returns or sets the value indicating if open edges of the revolve mesh can be sewn with selected input open edges.
-------------------------------------
Getter Method
Signature
CanSew
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanSew
Parameters: canSew (bool) – New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Continuity¶
-
SubdivisionRevolveBuilder.
Continuity
¶ Returns or sets the continuity.
The continuity is used to specify creases in the limit surface corresponding to edges of the revolved region that are sewn with the primary existing region.
-------------------------------------
Getter Method
Signature
Continuity
Returns: Return type: NXOpen.Features.Subdivision.SubdivisionRevolveBuilderContinuityType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Continuity
Parameters: continuity ( NXOpen.Features.Subdivision.SubdivisionRevolveBuilderContinuityType
) –New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
EndAngle¶
-
SubdivisionRevolveBuilder.
EndAngle
¶ Returns the end of angular dimension.
-------------------------------------
Getter Method
Signature
EndAngle
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
NumOfSegments¶
-
SubdivisionRevolveBuilder.
NumOfSegments
¶ Returns or sets the number of segments.
-------------------------------------
Getter Method
Signature
NumOfSegments
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumOfSegments
Parameters: numOfSegments (int) – New in version NX10.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
SectionObject¶
-
SubdivisionRevolveBuilder.
SectionObject
¶ Returns the section as revolving profile.
-------------------------------------
Getter Method
Signature
SectionObject
Returns: Return type: NXOpen.Features.Subdivision.SelectCageObjectData
New in version NX10.0.0.
License requirements: None.
StartAngle¶
-
SubdivisionRevolveBuilder.
StartAngle
¶ Returns the start of angular dimension.
-------------------------------------
Getter Method
Signature
StartAngle
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SubdivisionRevolveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.