SubdivisionFillBuilder Class¶
-
class
NXOpen.Features.Subdivision.
SubdivisionFillBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.Subdivision.SubdivisionFillBuilder
builder.To create a new instance of this class, use
NXOpen.Features.Subdivision.SubdivisionBodyCollection.CreateSubdivisionFillBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CanConnectSymmetrically | Returns or sets the flag indicating if selected edges are to be connected with their symmetric counterpart. |
Continuity | Returns or sets the continuity. |
SelectedEdges | Returns the edges to form a face. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SubdivisionFillBuilderContinuityType Enumeration | Type of continuity. |
Property Detail¶
CanConnectSymmetrically¶
-
SubdivisionFillBuilder.
CanConnectSymmetrically
¶ Returns or sets the flag indicating if selected edges are to be connected with their symmetric counterpart.
-------------------------------------
Getter Method
Signature
CanConnectSymmetrically
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanConnectSymmetrically
Parameters: connectSymmetrically (bool) – New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Continuity¶
-
SubdivisionFillBuilder.
Continuity
¶ Returns or sets the continuity.
The continuity is used to specify creases in the limit surface corresponding to edges specified by
NXOpen.Features.Subdivision.SubdivisionFillBuilder.SelectedEdges()
.-------------------------------------
Getter Method
Signature
Continuity
Returns: Return type: NXOpen.Features.Subdivision.SubdivisionFillBuilderContinuityType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Continuity
Parameters: continuity ( NXOpen.Features.Subdivision.SubdivisionFillBuilderContinuityType
) –New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
SelectedEdges¶
-
SubdivisionFillBuilder.
SelectedEdges
¶ Returns the edges to form a face.
-------------------------------------
Getter Method
Signature
SelectedEdges
Returns: Return type: NXOpen.Features.Subdivision.SelectCageObjectData
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SubdivisionFillBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.