SketchConversionStatus Class¶
-
class
NXOpen.Features.
SketchConversionStatus
¶ Bases:
NXOpen.TransientObject
Represents the status of conversion of features to independent sketch.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Feature | Returns the feature being converted to independent sketch. |
Reason | Returns the reason for failed or partially succeeded conversion of a linked-feature to an independent sketch |
Status | Returns the status of conversion of a feature to an independent sketch. |
Enumerations¶
SketchConversionStatusReasonType Enumeration | Reason for partial-success or failure of conversion to sketch |
SketchConversionStatusType Enumeration | Status of conversion - Success, Failure or Partial-Success |
Property Detail¶
Feature¶
-
SketchConversionStatus.
Feature
¶ Returns the feature being converted to independent sketch.
-------------------------------------
Getter Method
Signature
Feature
Returns: Return type: NXOpen.Features.Feature
New in version NX7.5.0.
License requirements: None.
Reason¶
-
SketchConversionStatus.
Reason
¶ Returns the reason for failed or partially succeeded conversion of a linked-feature to an independent sketch
-------------------------------------
Getter Method
Signature
Reason
Returns: Return type: NXOpen.Features.SketchConversionStatusReasonType
New in version NX7.5.0.
License requirements: None.
Status¶
-
SketchConversionStatus.
Status
¶ Returns the status of conversion of a feature to an independent sketch.
-------------------------------------
Getter Method
Signature
Status
Returns: Return type: NXOpen.Features.SketchConversionStatusType
New in version NX7.5.0.
License requirements: None.