WeldCutBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
WeldCutBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.WeldCut
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateWeldCutBuilder()
Default values.
Property Value SketchBlock.Exp1.Value 0 SketchBlock.Exp10.Value 0 SketchBlock.Exp11.Value 0 SketchBlock.Exp12.Value 0 SketchBlock.Exp2.Value 0 SketchBlock.Exp3.Value 0 SketchBlock.Exp4.Value 0 SketchBlock.Exp5.Value 0 SketchBlock.Exp6.Value 0 SketchBlock.Exp7.Value 0 SketchBlock.Exp8.Value 0 SketchBlock.Exp9.Value 0 SketchBlock.Sketches EndCut1 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
CoordSystem | Returns or sets the placement CSYS of the weld cut The coordinate system is only used for the SpecifyCSYS placement method. |
KeepCoordSystem | Returns or sets the keep coordinate system. |
KeepSelectCSYSFace | Returns or sets the keep select target face. |
KeepSelectGuideCurve | Returns or sets the keep select guide curve. |
KeepSelectTargetFace | Returns or sets the keep select target face. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlacementType | Returns or sets the method used to define the placement of the weld cut |
SelectCSYSFace | Returns the selection object for the target face. |
SelectGuideCurve | Returns the selection object for the guide curve. |
SelectTargetFace | Returns the selection object for the target face. |
SketchBlock | Returns the sketch block |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
WeldLocation | Returns or sets the weld location. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WeldCutBuilderCreationMethod Enumeration | Creation method used to define the placement of the weld cut |
Property Detail¶
CoordSystem¶
-
WeldCutBuilder.
CoordSystem
¶ Returns or sets the placement CSYS of the weld cut The coordinate system is only used for the SpecifyCSYS placement method.
-------------------------------------
Getter Method
Signature
CoordSystem
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordSystem
Parameters: coordSystem ( NXOpen.CoordinateSystem
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepCoordSystem¶
-
WeldCutBuilder.
KeepCoordSystem
¶ Returns or sets the keep coordinate system.
A toggle used to remember the specified csys on apply. The keep selected coordinate system is only used for the SpecifyCSYS placement method.
-------------------------------------
Getter Method
Signature
KeepCoordSystem
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepCoordSystem
Parameters: keepCoordSystem (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepSelectCSYSFace¶
-
WeldCutBuilder.
KeepSelectCSYSFace
¶ Returns or sets the keep select target face.
A toggle used to remember the selected target face on apply. This keep select target face is only used for the SpecifyCSYS placement method.
-------------------------------------
Getter Method
Signature
KeepSelectCSYSFace
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepSelectCSYSFace
Parameters: keepSelectCSYSFace (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepSelectGuideCurve¶
-
WeldCutBuilder.
KeepSelectGuideCurve
¶ Returns or sets the keep select guide curve.
A toggle used to remember the selected guide curve on apply. The keep select guide curve is only used for the AlongGuide placement method.
-------------------------------------
Getter Method
Signature
KeepSelectGuideCurve
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepSelectGuideCurve
Parameters: keepSelectGuideCurve (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepSelectTargetFace¶
-
WeldCutBuilder.
KeepSelectTargetFace
¶ Returns or sets the keep select target face.
A toggle used to remember the selected target face on apply. This keep select target face is only used for the AlongGuide placement method.
-------------------------------------
Getter Method
Signature
KeepSelectTargetFace
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepSelectTargetFace
Parameters: keepSelectTargetFace (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
PlacementType¶
-
WeldCutBuilder.
PlacementType
¶ Returns or sets the method used to define the placement of the weld cut
-------------------------------------
Getter Method
Signature
PlacementType
Returns: Return type: NXOpen.Features.ShipDesign.WeldCutBuilderCreationMethod
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlacementType
Parameters: placementType ( NXOpen.Features.ShipDesign.WeldCutBuilderCreationMethod
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
SelectCSYSFace¶
-
WeldCutBuilder.
SelectCSYSFace
¶ Returns the selection object for the target face.
This target face is only used for the SpecifyCSYS placement method.
-------------------------------------
Getter Method
Signature
SelectCSYSFace
Returns: Return type: NXOpen.SelectFace
New in version NX7.5.0.
License requirements: None.
SelectGuideCurve¶
-
WeldCutBuilder.
SelectGuideCurve
¶ Returns the selection object for the guide curve.
The select guide curve is only used for the AlongGuide placement method.
-------------------------------------
Getter Method
Signature
SelectGuideCurve
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX7.5.0.
License requirements: None.
SelectTargetFace¶
-
WeldCutBuilder.
SelectTargetFace
¶ Returns the selection object for the target face.
This target face is only used for the AlongGuide placement method.
-------------------------------------
Getter Method
Signature
SelectTargetFace
Returns: Return type: NXOpen.SelectFace
New in version NX7.5.0.
License requirements: None.
SketchBlock¶
-
WeldCutBuilder.
SketchBlock
¶ Returns the sketch block
-------------------------------------
Getter Method
Signature
SketchBlock
Returns: Return type: NXOpen.SketchExpressionModifierBuilder
New in version NX7.5.0.
License requirements: None.
WeldLocation¶
-
WeldCutBuilder.
WeldLocation
¶ Returns or sets the weld location.
The weld location is only used for the Corner placement method.
-------------------------------------
Getter Method
Signature
WeldLocation
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WeldLocation
Parameters: weldLocation ( NXOpen.Point
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
WeldCutBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.