SubSystemBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
SubSystemBuilder
¶ Bases:
NXOpen.Features.ShipDesign.FeatureParmsBuilder
This class is used to edit the Sub System Definition of a
NXOpen.Features.ShipDesign.SubSystems
feature.No creator since only created along with Features.ShipDesign.SubSystemsBuilder
Default values.
Property Value PlateStockData.KnuckleRatio 3.0 PlateStockData.KnuckleSmoothAngle 3.0 PlateStockData.MaterialOption 0 PlateStockData.OppositeThickness.Value 0 (millimeters part), 0 (inches part) PlateStockData.RestrictThicknessToMaterial true PlateStockData.ThickenOption SingleSided PlateStockData.Thickness.Value 10 (millimeters part), 0.5 (inches part) PlateStockData.ThicknessSourceOption List ProfileStockData.AnchorPoint 0 ProfileStockData.PlateHeight.Value 50 (millimeters part), 2 (inches part) ProfileStockData.SectionType Profile New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the tolerance, in degrees, used to determine when angles are zero. |
DistanceTolerance | Returns or sets the tolerance used to determine when distances are considered zero. |
EndCutEnd | Returns or sets the end cut to use at the end of the stiffener sub system. |
EndCutStart | Returns or sets the end cut to use at the start of the stiffener sub system. |
MountingMethod | Returns or sets the mounting method |
Name | Returns or sets the name of the Subsystem and the name of the part created for the SubSystem by Transition |
Offset | Returns the offset to apply to the plate sub system mold face to produce the desired mold face. |
OrientationAngle | Returns the angle at which the stiffener system is placed relative to the reference. |
OrientationAngleRule | Returns or sets the angle rule to use when measuring angles. |
OrientationLinePillar | Returns the line specified for the pillar system angle reference. |
OrientationMethod | Returns or sets the method used to define the reference for the orientation angle of stiffener system. |
OrientationVector | Returns or sets the vector specified for the orientation angle reference. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PillarStockData | Returns the pillar sub system stock data. |
PlateStockData | Returns the plate sub system stock data. |
ProfileStockData | Returns the profile sub system stock data. |
Reverse | Returns or sets the indication whether the direction of the flange should be reversed on this stiffener sub system. |
SubSystem | Returns the faces or curves that make up the sub system. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tightness | Returns or sets the tightness to apply to plate and subplate systems. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreatePlaneForList | Create a NXOpen.Features.ShipDesign.PlaneListBuilder to add a defined plane to a list. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EndCutEnd¶
-
SubSystemBuilder.
EndCutEnd
¶ Returns or sets the end cut to use at the end of the stiffener sub system.
-------------------------------------
Getter Method
Signature
EndCutEnd
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCutEnd
Parameters: endCutEnd ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
) –New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
EndCutStart¶
-
SubSystemBuilder.
EndCutStart
¶ Returns or sets the end cut to use at the start of the stiffener sub system.
-------------------------------------
Getter Method
Signature
EndCutStart
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCutStart
Parameters: endCutStart ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderEndCutTypes
) –New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
MountingMethod¶
-
SubSystemBuilder.
MountingMethod
¶ Returns or sets the mounting method
-------------------------------------
Getter Method
Signature
MountingMethod
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderMountingMethods
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MountingMethod
Parameters: mountingMethod ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderMountingMethods
) –New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Name¶
-
SubSystemBuilder.
Name
¶ Returns or sets the name of the Subsystem and the name of the part created for the SubSystem by Transition
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX8.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Offset¶
-
SubSystemBuilder.
Offset
¶ Returns the offset to apply to the plate sub system mold face to produce the desired mold face.
The offset is applied in the thickness direction specified.
-------------------------------------
Getter Method
Signature
Offset
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OrientationAngle¶
-
SubSystemBuilder.
OrientationAngle
¶ Returns the angle at which the stiffener system is placed relative to the reference.
-------------------------------------
Getter Method
Signature
OrientationAngle
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
OrientationLinePillar¶
-
SubSystemBuilder.
OrientationLinePillar
¶ Returns the line specified for the pillar system angle reference.
-------------------------------------
Getter Method
Signature
OrientationLinePillar
Returns: Return type: NXOpen.SelectCurve
New in version NX8.5.0.
License requirements: None.
OrientationMethod¶
-
SubSystemBuilder.
OrientationMethod
¶ Returns or sets the method used to define the reference for the orientation angle of stiffener system.
-------------------------------------
Getter Method
Signature
OrientationMethod
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerSystemBuilderOrientationMethods
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationMethod
Parameters: orientationMethod ( NXOpen.Features.ShipDesign.StiffenerSystemBuilderOrientationMethods
) –New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
OrientationVector¶
-
SubSystemBuilder.
OrientationVector
¶ Returns or sets the vector specified for the orientation angle reference.
Only used when when Method is
NXOpen.Features.ShipDesign.StiffenerSystemBuilderOrientationMethods.Vector
..-------------------------------------
Getter Method
Signature
OrientationVector
Returns: Return type: NXOpen.Direction
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationVector
Parameters: orientationVector ( NXOpen.Direction
) –New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
PillarStockData¶
-
SubSystemBuilder.
PillarStockData
¶ Returns the pillar sub system stock data.
-------------------------------------
Getter Method
Signature
PillarStockData
Returns: Pillar Stock Builder Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX8.0.0.
License requirements: None.
PlateStockData¶
-
SubSystemBuilder.
PlateStockData
¶ Returns the plate sub system stock data.
-------------------------------------
Getter Method
Signature
PlateStockData
Returns: Plate Stock Builder Return type: NXOpen.Features.ShipDesign.PlateStockBuilder
New in version NX8.0.0.
License requirements: None.
ProfileStockData¶
-
SubSystemBuilder.
ProfileStockData
¶ Returns the profile sub system stock data.
-------------------------------------
Getter Method
Signature
ProfileStockData
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerStockBuilder
New in version NX8.0.0.
License requirements: None.
Reverse¶
-
SubSystemBuilder.
Reverse
¶ Returns or sets the indication whether the direction of the flange should be reversed on this stiffener sub system.
The default direction is based on the ship structure that the stiffener is being built upon.
-------------------------------------
Getter Method
Signature
Reverse
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Reverse
Parameters: reverse (bool) – New in version NX8.5.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
SubSystem¶
-
SubSystemBuilder.
SubSystem
¶ Returns the faces or curves that make up the sub system.
-------------------------------------
Getter Method
Signature
SubSystem
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
Tightness¶
-
SubSystemBuilder.
Tightness
¶ Returns or sets the tightness to apply to plate and subplate systems.
-------------------------------------
Getter Method
Signature
Tightness
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tightness
Parameters: tightness (int) – New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Method Detail¶
Validate¶
-
SubSystemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.