ShipSectionBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ShipSectionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.ShipSection
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateShipSectionBuilder()
Default values.
Property Value ReadDataSet.CreateDataSetToggle 0 ReadDataSet.NativeToggle 0 XDatumFilter All XMaxOffset.Value 0 (millimeters part), 0 (inches part) XMinOffset.Value 0 (millimeters part), 0 (inches part) YMaxOffset.Value 0 (millimeters part), 0 (inches part) YMinOffset.Value 0 (millimeters part), 0 (inches part) ZDatumFilter All ZMaxOffset.Value 0 (millimeters part), 0 (inches part) ZMinOffset.Value 0 (millimeters part), 0 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AssemblyPart | Returns or sets the assembly part |
BottomDeckSectionName | Returns or sets the bottom deck section name |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReadDataSet | Returns the Data Set Builder for reading data sets from Team Center |
ReferenceGeometry | Returns the reference geometry |
SectionName | Returns or sets the section name |
SectionPart | Returns or sets the section part |
SectionType | Returns or sets the creation method |
SectionXMax | Returns or sets the section xmax |
SectionXMin | Returns or sets the section xmin |
SectionYMax | Returns or sets the section ymax |
SectionYMin | Returns or sets the section ymin |
SectionZMax | Returns or sets the section zmax |
SectionZMin | Returns or sets the section zmin |
ShipBodies | Returns the ship bodies |
ShipBody | Returns the ship body |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
XDatumFilter | Returns or sets the x datum filter |
XMaxDatumFilter | Returns or sets the x max datum filter |
XMaxOffset | Returns the x max offset |
XMinDatumFilter | Returns or sets the x min datum filter |
XMinOffset | Returns the x min offset |
YDatumFilter | Returns or sets the y datum filter |
YMaxDatumFilter | Returns or sets the y max datum filter |
YMaxOffset | Returns the y max offset |
YMinDatumFilter | Returns or sets the y min datum filter |
YMinOffset | Returns the y min offset |
ZDatumFilter | Returns or sets the z datum filter |
ZMaxDatumFilter | Returns or sets the z max datum filter |
ZMaxOffset | Returns the z max offset |
ZMinDatumFilter | Returns or sets the z min datum filter |
ZMinOffset | Returns the z min offset |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetDeckContainer | Sets the deck container flag |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ShipSectionBuilderType Enumeration | Define the creation type |
ShipSectionBuilderXFilter Enumeration | Define the output option for each of the frame type |
ShipSectionBuilderZFilter Enumeration | Define the output option for each of the frame type |
Property Detail¶
AssemblyPart¶
-
ShipSectionBuilder.
AssemblyPart
¶ Returns or sets the assembly part
-------------------------------------
Getter Method
Signature
AssemblyPart
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssemblyPart
Parameters: filename (str) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
BottomDeckSectionName¶
-
ShipSectionBuilder.
BottomDeckSectionName
¶ Returns or sets the bottom deck section name
-------------------------------------
Getter Method
Signature
BottomDeckSectionName
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BottomDeckSectionName
Parameters: bottomSectionName (str) – New in version NX12.0.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
ReadDataSet¶
-
ShipSectionBuilder.
ReadDataSet
¶ Returns the Data Set Builder for reading data sets from Team Center
-------------------------------------
Getter Method
Signature
ReadDataSet
Returns: Return type: NXOpen.Features.ShipDesign.ReadDataSetBuilder
New in version NX8.5.0.
License requirements: None.
ReferenceGeometry¶
-
ShipSectionBuilder.
ReferenceGeometry
¶ Returns the reference geometry
-------------------------------------
Getter Method
Signature
ReferenceGeometry
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX10.0.0.
License requirements: None.
SectionName¶
-
ShipSectionBuilder.
SectionName
¶ Returns or sets the section name
-------------------------------------
Getter Method
Signature
SectionName
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionName
Parameters: sectionName (str) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionPart¶
-
ShipSectionBuilder.
SectionPart
¶ Returns or sets the section part
-------------------------------------
Getter Method
Signature
SectionPart
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionPart
Parameters: filename (str) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionType¶
-
ShipSectionBuilder.
SectionType
¶ Returns or sets the creation method
-------------------------------------
Getter Method
Signature
SectionType
Returns: Return type: NXOpen.Features.ShipDesign.ShipSectionBuilderType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionType
Parameters: type ( NXOpen.Features.ShipDesign.ShipSectionBuilderType
) –New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionXMax¶
-
ShipSectionBuilder.
SectionXMax
¶ Returns or sets the section xmax
-------------------------------------
Getter Method
Signature
SectionXMax
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionXMax
Parameters: sectionXMax (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionXMin¶
-
ShipSectionBuilder.
SectionXMin
¶ Returns or sets the section xmin
-------------------------------------
Getter Method
Signature
SectionXMin
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionXMin
Parameters: sectionXMin (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionYMax¶
-
ShipSectionBuilder.
SectionYMax
¶ Returns or sets the section ymax
-------------------------------------
Getter Method
Signature
SectionYMax
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionYMax
Parameters: sectionYMax (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionYMin¶
-
ShipSectionBuilder.
SectionYMin
¶ Returns or sets the section ymin
-------------------------------------
Getter Method
Signature
SectionYMin
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionYMin
Parameters: sectionYMin (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionZMax¶
-
ShipSectionBuilder.
SectionZMax
¶ Returns or sets the section zmax
-------------------------------------
Getter Method
Signature
SectionZMax
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionZMax
Parameters: sectionZMax (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
SectionZMin¶
-
ShipSectionBuilder.
SectionZMin
¶ Returns or sets the section zmin
-------------------------------------
Getter Method
Signature
SectionZMin
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionZMin
Parameters: sectionZMin (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
ShipBodies¶
-
ShipSectionBuilder.
ShipBodies
¶ Returns the ship bodies
-------------------------------------
Getter Method
Signature
ShipBodies
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX12.0.0.
License requirements: None.
ShipBody¶
-
ShipSectionBuilder.
ShipBody
¶ Returns the ship body
-------------------------------------
Getter Method
Signature
ShipBody
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
XDatumFilter¶
-
ShipSectionBuilder.
XDatumFilter
¶ Returns or sets the x datum filter
-------------------------------------
Getter Method
Signature
XDatumFilter
Returns: Return type: NXOpen.Features.ShipDesign.ShipSectionBuilderXFilter
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XDatumFilter
Parameters: xDatumFilter ( NXOpen.Features.ShipDesign.ShipSectionBuilderXFilter
) –New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
XMaxDatumFilter¶
-
ShipSectionBuilder.
XMaxDatumFilter
¶ Returns or sets the x max datum filter
-------------------------------------
Getter Method
Signature
XMaxDatumFilter
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XMaxDatumFilter
Parameters: xMaxDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
XMaxOffset¶
-
ShipSectionBuilder.
XMaxOffset
¶ Returns the x max offset
-------------------------------------
Getter Method
Signature
XMaxOffset
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
XMinDatumFilter¶
-
ShipSectionBuilder.
XMinDatumFilter
¶ Returns or sets the x min datum filter
-------------------------------------
Getter Method
Signature
XMinDatumFilter
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XMinDatumFilter
Parameters: xMinDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
XMinOffset¶
-
ShipSectionBuilder.
XMinOffset
¶ Returns the x min offset
-------------------------------------
Getter Method
Signature
XMinOffset
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
YDatumFilter¶
-
ShipSectionBuilder.
YDatumFilter
¶ Returns or sets the y datum filter
-------------------------------------
Getter Method
Signature
YDatumFilter
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YDatumFilter
Parameters: yDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
YMaxDatumFilter¶
-
ShipSectionBuilder.
YMaxDatumFilter
¶ Returns or sets the y max datum filter
-------------------------------------
Getter Method
Signature
YMaxDatumFilter
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YMaxDatumFilter
Parameters: yMaxDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
YMaxOffset¶
-
ShipSectionBuilder.
YMaxOffset
¶ Returns the y max offset
-------------------------------------
Getter Method
Signature
YMaxOffset
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
YMinDatumFilter¶
-
ShipSectionBuilder.
YMinDatumFilter
¶ Returns or sets the y min datum filter
-------------------------------------
Getter Method
Signature
YMinDatumFilter
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YMinDatumFilter
Parameters: yMinDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
YMinOffset¶
-
ShipSectionBuilder.
YMinOffset
¶ Returns the y min offset
-------------------------------------
Getter Method
Signature
YMinOffset
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ZDatumFilter¶
-
ShipSectionBuilder.
ZDatumFilter
¶ Returns or sets the z datum filter
-------------------------------------
Getter Method
Signature
ZDatumFilter
Returns: Return type: NXOpen.Features.ShipDesign.ShipSectionBuilderZFilter
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZDatumFilter
Parameters: zDatumFilter ( NXOpen.Features.ShipDesign.ShipSectionBuilderZFilter
) –New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
ZMaxDatumFilter¶
-
ShipSectionBuilder.
ZMaxDatumFilter
¶ Returns or sets the z max datum filter
-------------------------------------
Getter Method
Signature
ZMaxDatumFilter
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZMaxDatumFilter
Parameters: zMaxDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
ZMaxOffset¶
-
ShipSectionBuilder.
ZMaxOffset
¶ Returns the z max offset
-------------------------------------
Getter Method
Signature
ZMaxOffset
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ZMinDatumFilter¶
-
ShipSectionBuilder.
ZMinDatumFilter
¶ Returns or sets the z min datum filter
-------------------------------------
Getter Method
Signature
ZMinDatumFilter
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZMinDatumFilter
Parameters: zMinDatumFilter (int) – New in version NX7.5.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”) OR nx_ship_concept (“Ship Concept”) OR nx_ship_detail (“Ship Detail Design”)
ZMinOffset¶
-
ShipSectionBuilder.
ZMinOffset
¶ Returns the z min offset
-------------------------------------
Getter Method
Signature
ZMinOffset
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Method Detail¶
SetDeckContainer¶
-
ShipSectionBuilder.
SetDeckContainer
¶ Sets the deck container flag
Signature
SetDeckContainer(isDeckContainer)
Parameters: isDeckContainer (bool) – New in version NX12.0.0.
License requirements: None.
Validate¶
-
ShipSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.