ShipIntersectionsBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ShipIntersectionsBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.ShipIntersections
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateShipIntersectionsBuilder()
Default values.
Property Value BulkheadEnum None DeckEnum None InterTransFrameEnum None ReadDataSet.CreateDataSetToggle 0 ReadDataSet.NativeToggle 0 TransFrameEnum None YFrameEnum None ZFrameEnum None New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
BulkheadEnum | Returns or sets the output option for the Bulkhead Frames |
DeckEnum | Returns or sets the output option for the Longitudinal Z Frames |
InterSectionsType | Returns or sets the creation method |
InterTransFrameEnum | Returns or sets the output option for the Inter Transverse Frames |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReadDataSet | Returns the Data Set Builder for reading data sets from Team Center |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TransFrameEnum | Returns or sets the output option for the Transverse Frames |
YFrameEnum | Returns or sets the output option for the Longitudinal Y Frames |
ZFrameEnum | Returns or sets the output option for the Longitudinal Z Frames |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ShipIntersectionsBuilderCreationType Enumeration | Define the creation type |
ShipIntersectionsBuilderType Enumeration | Define the output option for each of the frame type |
Property Detail¶
BulkheadEnum¶
-
ShipIntersectionsBuilder.
BulkheadEnum
¶ Returns or sets the output option for the Bulkhead Frames
-------------------------------------
Getter Method
Signature
BulkheadEnum
Returns: Return type: NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BulkheadEnum
Parameters: bulkheadEnum ( NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
DeckEnum¶
-
ShipIntersectionsBuilder.
DeckEnum
¶ Returns or sets the output option for the Longitudinal Z Frames
-------------------------------------
Getter Method
Signature
DeckEnum
Returns: Return type: NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeckEnum
Parameters: deckEnum ( NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
InterSectionsType¶
-
ShipIntersectionsBuilder.
InterSectionsType
¶ Returns or sets the creation method
-------------------------------------
Getter Method
Signature
InterSectionsType
Returns: Return type: NXOpen.Features.ShipDesign.ShipIntersectionsBuilderCreationType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterSectionsType
Parameters: type ( NXOpen.Features.ShipDesign.ShipIntersectionsBuilderCreationType
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
InterTransFrameEnum¶
-
ShipIntersectionsBuilder.
InterTransFrameEnum
¶ Returns or sets the output option for the Inter Transverse Frames
-------------------------------------
Getter Method
Signature
InterTransFrameEnum
Returns: Return type: NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterTransFrameEnum
Parameters: interTransFrameEnum ( NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
ReadDataSet¶
-
ShipIntersectionsBuilder.
ReadDataSet
¶ Returns the Data Set Builder for reading data sets from Team Center
-------------------------------------
Getter Method
Signature
ReadDataSet
Returns: Return type: NXOpen.Features.ShipDesign.ReadDataSetBuilder
New in version NX8.5.0.
License requirements: None.
TransFrameEnum¶
-
ShipIntersectionsBuilder.
TransFrameEnum
¶ Returns or sets the output option for the Transverse Frames
-------------------------------------
Getter Method
Signature
TransFrameEnum
Returns: Return type: NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransFrameEnum
Parameters: transFrameEnum ( NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
YFrameEnum¶
-
ShipIntersectionsBuilder.
YFrameEnum
¶ Returns or sets the output option for the Longitudinal Y Frames
-------------------------------------
Getter Method
Signature
YFrameEnum
Returns: Return type: NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YFrameEnum
Parameters: yFrameEnum ( NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
ZFrameEnum¶
-
ShipIntersectionsBuilder.
ZFrameEnum
¶ Returns or sets the output option for the Longitudinal Z Frames
-------------------------------------
Getter Method
Signature
ZFrameEnum
Returns: Return type: NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZFrameEnum
Parameters: zFrameEnum ( NXOpen.Features.ShipDesign.ShipIntersectionsBuilderType
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Method Detail¶
Validate¶
-
ShipIntersectionsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.