RoomPanelBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
RoomPanelBuilder
¶ Bases:
NXOpen.Builder
Represents a
Features.ShipDesign.RoomPanelBuilder
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateRoomPanelBuilder()
Default values.
Property Value Thickness.Value 7 (millimeters part), 0.25 (inches part) New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
AdoptBodySelect | Returns the adopt body select |
PanelSketchSection | Returns the panel sketch section |
RoomBodySelect | Returns the room body select |
Tag | Returns the Tag for this object. |
Thickness | Returns the thickness |
Tolerance | Returns or sets the tolerance |
Type | Returns or sets the type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RoomPanelBuilderTypes Enumeration | Represents the type |
Property Detail¶
AdoptBodySelect¶
-
RoomPanelBuilder.
AdoptBodySelect
¶ Returns the adopt body select
-------------------------------------
Getter Method
Signature
AdoptBodySelect
Returns: Return type: NXOpen.ScCollector
New in version NX12.0.0.
License requirements: None.
PanelSketchSection¶
-
RoomPanelBuilder.
PanelSketchSection
¶ Returns the panel sketch section
-------------------------------------
Getter Method
Signature
PanelSketchSection
Returns: Return type: NXOpen.Section
New in version NX12.0.0.
License requirements: None.
RoomBodySelect¶
-
RoomPanelBuilder.
RoomBodySelect
¶ Returns the room body select
-------------------------------------
Getter Method
Signature
RoomBodySelect
Returns: Return type: NXOpen.ScCollector
New in version NX12.0.0.
License requirements: None.
Thickness¶
-
RoomPanelBuilder.
Thickness
¶ Returns the thickness
-------------------------------------
Getter Method
Signature
Thickness
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: None.
Tolerance¶
-
RoomPanelBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: tolerance (float) – New in version NX12.0.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”)
Type¶
-
RoomPanelBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.ShipDesign.RoomPanelBuilderTypes
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.ShipDesign.RoomPanelBuilderTypes
) –New in version NX12.0.0.
License requirements: nx_ship_gen_arrange (“Ship General Arrangement”)
Method Detail¶
Validate¶
-
RoomPanelBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.